2021-06-14 8:08 PM
Hi,
My test kit is STM32MP157C-DK2 and kenerl version is 5.10.10.
I tried to monitor falling edge event on PD.1, with command "gpiomon --falling-edge gpiochip3 1".
It is faile and and the log in the attachment.
Then I disable "hdmi-transmitter@39" in "stm32mp15xx-dkx.dtsi" and comiple it again and replace file in the OS, Then executing command "gpiomon --falling-edge gpiochip3 1" will work correctly.
Please advise why PIN PG.1 interrupt configuration will affect PIN PD.1 interrupt configuration.
Thanks,
QiZhang
Solved! Go to Solution.
2021-06-16 12:18 AM
Hi,
this is due to EXTI constrain on muxing from pins,
See https://wiki.st.com/stm32mpu/wiki/EXTI_internal_peripheral
"Up to 16 GPIO pins can be configured as external interrupts: for each index between 0 and 15, one EXTI can be selected among all banks (EXTI<index> = GPIO<one_bank><index>)."
Regards.
2021-06-16 12:18 AM
Hi,
this is due to EXTI constrain on muxing from pins,
See https://wiki.st.com/stm32mpu/wiki/EXTI_internal_peripheral
"Up to 16 GPIO pins can be configured as external interrupts: for each index between 0 and 15, one EXTI can be selected among all banks (EXTI<index> = GPIO<one_bank><index>)."
Regards.
2021-06-16 5:24 AM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'