2022-04-06 4:27 AM
Could you explain to me what is the purpose of the different bits associated to the tampers?
I am mainly focus on using the passive tampers of the STM32MP1 and I have seen the following configuration bits I don't fully understand:
What I understand:
What I am confused about:
Another configuration bit I would like to clarify is "TAMPDPROT", changing this bit I could trigger the interrupt in the Secure Context in Sp-Min, but not in Non-Secure Context in Linux. This is probably because of some configuration missing in the Linux environment, How could I configure the linux to react to the interrupt? Printing a message for example...
Does the "TAMPDPROT" bit, limit the access and interaction, including the configuration registers and interrupt handler, to the secure context vs non-secure context?
Best regards,
Andrés
2022-05-19 5:07 AM
Hello
Regarding the request to handle tamper interrupt into non secure Linux I think you may refer to below post:
https://community.st.com/s/question/0D53W000013qHGlSAM/how-detect-and-store-tamper-event-by-linux
Regarding TAMPER bits let me come back to you in the next days.
JM
2022-05-19 5:37 AM
also..
The TAMPxMSK can be used in low power mode to avoid system wakeup to clear the TAMPxF flag as stated in the RM Section “Trigger output generation on tamper event�?
When TAMPxMSK bit is set, the TAMPxF flag is masked, and kept cleared in TAMP_SR
register. This configuration permits the low-power timers to be triggered automatically in
Stop mode, without requiring the system wakeup to perform the TAMPxF clearing. In this
case, the backup registers are not cleared.
As stated above, those are 2 different ways to use the tamper. It is either using TAMPxMASK (when in low power mode mainly) or using TAMPxIE
The TAMP_MISR register is read only. So yes only flags. They are set when the corresponding interrupt is raised.
Yes same as TAMP_MISR for secure.
Yes. When set to 0 only secure APB access are allowed to configure the tamper.
JM
2022-05-20 12:17 AM
small additional info:
the TAMP_MISR and TAMP_SMISR are flag that are only active when the iterrupt is enabled
and so are must be used in the ISR interrupt routines.
the TAMP_SR are flags that will be activated independently of the interrupt activation.
JM