2023-02-15 4:16 AM
2023-02-20 1:30 AM
Hi @VUnni.1
to complete the answer from @Kevin HUBER , any "USB Type-C compliant" supply rated above 5V/3A will work.
Supply rated 5V/3A , 9V/2.77A (or above) will work as well. Per USB standard, supply must start with a default 5V when pull-down on CC line is detected. The 9V or above voltage will be enabled only after successful 'power delivery' negotiation (which obviously is not done by STM32MP157x-DKx boards).
Even if rated 5V/3A, supply with Type-A socket with a Type-A <-> Type-C cable are usually showing warning (blinking led) but could work (but sometimes not recognized and uboot will stop).
This (old) post could help you.
https://community.st.com/s/question/0D50X0000Bftr1ySQA/power-supply-for-stm32mp157cdk2
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-02-15 8:47 AM
Hello @VUnni.1 ,
If you look at the user manual of your board page 10:
https://www.st.com/resource/en/user_manual/dm00652742-.pdf
It is recommended to
use a USB Type-C® to USB Type-C® 5 V/3 A charger.
Otherwise, we can't guarantee whether it will work or not.
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-02-20 1:30 AM
Hi @VUnni.1
to complete the answer from @Kevin HUBER , any "USB Type-C compliant" supply rated above 5V/3A will work.
Supply rated 5V/3A , 9V/2.77A (or above) will work as well. Per USB standard, supply must start with a default 5V when pull-down on CC line is detected. The 9V or above voltage will be enabled only after successful 'power delivery' negotiation (which obviously is not done by STM32MP157x-DKx boards).
Even if rated 5V/3A, supply with Type-A socket with a Type-A <-> Type-C cable are usually showing warning (blinking led) but could work (but sometimes not recognized and uboot will stop).
This (old) post could help you.
https://community.st.com/s/question/0D50X0000Bftr1ySQA/power-supply-for-stm32mp157cdk2
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'