2023-01-10 02:08 AM
2023-01-10 04:22 AM
Hi @BBoge.2
this bit is for ST internal development purposes, it is recommended to keep it at 0.
ROM code traces are described here and are the only way to debug 1st level boot issues: See https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer
Regards
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-01-10 04:22 AM
Hi @BBoge.2
this bit is for ST internal development purposes, it is recommended to keep it at 0.
ROM code traces are described here and are the only way to debug 1st level boot issues: See https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer
Regards
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-01-10 10:22 PM
Thank you.
That means if the device is already closed the debugging will also not work.