OpenSTLinux Distribution patch release V4.0.2 is available
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-26 6:33 AM
Hi MPU's Community,
A "minor"patch release 4.0.2 is available for OpenSTLinux Distribution package.
The corresponding oe-manifest tag is openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27.
It contains some fix of issues detected early after DV4.0.0 / openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15 release and you may face.
Here is the changelog :
V4.0.2 ecosystem release
o layers/meta-st/meta-st-openstlinux from [182b150] to [cbb3a2e]
- [Update] CONF: update distro to Yocto 4.0.2
- [Update] GSTREAMER1.0: update to 1.20.2
- [Update] SYSTEMD: update to 250.5
o layers/meta-st/meta-st-stm32mp from [d00d3a0] to [00c2494]
- [Update] CLASS: FLASHLAYOUT: correct bad exit of loop
- [Update] CONF: correct examples to used according to devicetree package
- [Update] CONF:WIC: align WIC file content with devicetree name
- [Update] GCNANO-USERLAND: add symlinks to shared libs in /usr/lib for SDK usage
- [Update] GCNANO-USERLAND: fix PACKAGECONFIG names to fill RPROVIDES libs
- [Update] libdrm: set PACKAGECONFIG based on stm32mpcommon
- [Update] mesa: drop dri from PACKAGECONFIG
- [Update] TF-A-STM32MP: cleanup obsolete files
- [Update] TF-A-STM32MP: update Makefile.sdk to use specific build folder per soc
o layers/meta-st/meta-st-stm32mp-addons from [1135de7] to [b0b00bc]
- [Update] Add SECURITY.md
- [Update] CONF: update layer for stm32mp13-mx machine
- [Update] MACHINE: adapt to kirkstone override new grammar
o layers/meta-st/scripts from [510c8b0] to [9d87d2d]
- [Update] Add SECURITY.md
It's recommend to refer to Minor release updates section at project start or in the case you are facing issues.
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Labels:
-
STM32MP15 Lines