2025-02-04 04:22 AM
openstLinux version:
1. en.SOURCES-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06
2. en.SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06
command:
$ cd tf-a-stm32mp-v2.10.5-stm32mp-r1
$ export FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifacts
$ make -f $PWD/../Makefile.sdk TF_A_DEVICETREE=stm32mp157d-openedv DEPLOYDIR=$FIP_DEPLOYDIR_ROOT/arm-trusted-firmware stm32 -j2
$ cd optee-os-stm32mp-4.0.0-stm32mp-r1
$ export FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifacts
$ make -f $PWD/../Makefile.sdk CFG_EMBED_DTB_SOURCE_FILE=stm32mp157d-openedv DEPLOYDIR=$FIP_DEPLOYDIR_ROOT/optee optee -j2
$ cd u-boot-stm32mp-v2023.10-stm32mp-r1
$ make -f $PWD/../Makefile.sdk ARCH=arm CROSS_COMPILE=arm-ostl-linux-gnueabi- DEVICE_TREE=stm32mp157d-openedv all -j2
tvs:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x00000000 arm-trusted-firmware/tf-a-stm32mp157d-openedv-optee-programmer-usb.stm32
- 0x03 fip-boot FIP none 0x00000000 fip/fip-stm32mp157d-openedv-optee-programmer-usb.bin
P 0x04 fsbl1 Binary mmc1 boot1 arm-trusted-firmware/tf-a-stm32mp157d-openedv-optee-emmc.stm32
P 0x05 fsbl2 Binary mmc1 boot2 arm-trusted-firmware/tf-a-stm32mp157d-openedv-optee-emmc.stm32
P 0x06 metadata1 FWU_MDATA mmc1 0x00080000 arm-trusted-firmware/metadata.bin
P 0x07 metadata2 FWU_MDATA mmc1 0x00100000 arm-trusted-firmware/metadata.bin
P 0x08 fip-a FIP mmc1 0x00180000 fip/fip-stm32mp157d-openedv-optee-programmer-usb.bin
PED 0x09 fip-b FIP mmc1 0x00580000 none
PED 0x0A u-boot-env ENV mmc1 0x00980000 none
P 0x10 bootfs System mmc1 0x00A00000 none
P 0x11 rootfs FileSystem mmc1 0x04A00000 none
op-tee error. I'm looking for suggestions as to how to try and debug this panic and/or how to fix it.
Solved! Go to Solution.
2025-02-06 04:51 AM
@GatienC Thank you for your reply.
I have made modifications to the device tree. Especially the regulator min microvolt value of vddcore, I believe it is a crucial modification.
2025-02-04 04:38 AM
2025-02-05 05:37 AM
Hello @leven,
Do you mind adding traces in the stm32_cpu_opp_init() function to highlight what function call is failing please?
You might be missing the PLL1 or the some cpu supply description in the device-tree.
Thanks,
Gatien
2025-02-06 04:51 AM
@GatienC Thank you for your reply.
I have made modifications to the device tree. Especially the regulator min microvolt value of vddcore, I believe it is a crucial modification.