cancel
Showing results for 
Search instead for 
Did you mean: 

New : STM32MP15 distribution for Android™ v1.0.0

Olivier GALLIEN
ST Employee

ST is please to announce the st-android-9.0.0-2019-09-27 tag compatible with Android 9.0.0 (Pie).

Main software component versions :

·       Android version v9.0.0 (AOSP android-9.0.0_r46 tag)

·       Kernel version v4.19.49 (AOSP common kernel) + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       TF-A version v2.0 + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       U-Boot version v2018.11 + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       OP-TEE version v3.3.0 + updates for STM32MP1 and associated boards (waiting upstream finalization)

·       STM32CubeMP1 FW v1.1.0

·       GCC version v8.2

·       openOCD version v0.10.0

·       GCnano version v6.2.4

ST want to warn that this delivery is provided as demonstrator/enabler with following limitation/restriction :

-       No Android CTS/VTS qualification

-       No performance optimization

-      Productization only through partner

The recommended configuration:

   Display @480p

    DDR32bit 1GB

 The STM32MP15X-EVAL includes by default a display @720p, which has impacts on performances.

Customer should not expect same level of performance than with an OctoCore at 2Ghz + High end GPU .

The Andoid AOSP aim to make application in adequation with platform usage target (typically not smartphone UI like application)

Production is only supported by our partner program: (https://www.st.com/content/st_com/en/partner/partner-program/partnerpage.html.

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
0 REPLIES 0