cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any STM MCU/MPU which can be used for computer vision applications

NPete.3
Associate

Is there any STM MCU/MPU which can be used for computer vision applications such as face recognition, Object detection/tracking? If so, how much flash memory required to process video with 5MP camera at 30FPS?

Is there any STM MCU/MPU which can be used for AR/VR applications?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Guru

The STM32MP series is more suited. But even more suited would be a full blown computer.

5MP * 30fps * 3bpp = 3.6 GBps. Not processing that on an MCU.

If you feel a post has answered your question, please click "Accept as Solution".
PatrickF
ST Employee

Hi @NPete.3​ 

please have a look to https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package

and more specifically https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_-_face_recognition_using_TensorFlow_Lite_C%2B%2B_API

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.