2019-08-29 8:23 AM
2019-09-02 8:37 AM
Hello RogerPaudex (Flybotix),
At this time we only support our own OpenSTLinux s/w distribution, therefore at present Raspbian won't run on the STM32MP1as is.
You will need to customize your project to interface with the FLIR camera sensor, to interface with the SPI and I2C ports (STM32CubeMx can do that, in addition with the device tree generation) as well as application examples in STM32Cube_FW_MP1 library for SPI and I2C use.
I hope it helps.
Best Regards,
Olivier