cancel
Showing results for 
Search instead for 
Did you mean: 

I made a stm32mp15x fsbl signing tool in C

milkylainen
Associate III

To detach signing from cube programmer I made an open source C signing tool, using openssl. Should be rather easy to use in various build environments.

https://github.com/milkylainen/stm32mp1sign

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Might be worth noting. Works on Edge.

Doesn't work with Firefox 103.0.2 in Linux or Firefox 103.0.2 in Windows.

FF in Windows was completely clean.

Will fix in Edge. Thanks.

View solution in original post

4 REPLIES 4
Olivier GALLIEN
ST Employee

Hi @milkylainen​ ,

Thanks for sharing this !

Can I suggest you to promote it also in the Share/Project area of this community?

This will help to reach a wider audience !

Thanks again !

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Olivier.

Sure. I'll add it there.

But right now https://community.st.com/s/project-submission is only rendering me a blank page with a header. Everything else works on the site? Temporary glitch?

Hi @milkylainen​ 

Work at my end. ( MS Edge)

Are you well logged ?

Can you try with another browser and/or after cleanup of cache/cookies.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Might be worth noting. Works on Edge.

Doesn't work with Firefox 103.0.2 in Linux or Firefox 103.0.2 in Windows.

FF in Windows was completely clean.

Will fix in Edge. Thanks.