2020-09-30 09:10 PM
I want to know how to specify the address to load Cortex-M4 firmware when U-Boot or Linux Kernel load the firmware of Cortex-M4 in Retention RAM.
And, how to specify the address to load Cortex-M4 firmware if I load the firmware of Cortex-M4 in Retention RAM and MCUSRAM separately?
In addition, if I load the firmware of Cortex-M4 in Retention RAM and MCUSRAM separately, is the swithing of RetentionRAM and MCUSRAM done by MPU without the programmer being aware of it?
Solved! Go to Solution.
2020-10-11 07:38 PM
2020-10-05 05:44 PM
Is this thread's support over...?
I would be very grateful if you could support me.
Best Regards.
H. Masuda
2020-10-11 07:38 PM
I close this thread because resolved this problem myself.
H. Masuda