cancel
Showing results for 
Search instead for 
Did you mean: 

How to Enable Secure Boot on STM32MP13?

Hardin_Jenner
Associate

Hello,

I am currently working on an STM32MP13-based project and need to implement a secure boot process for the application. I've gone through the reference manual and ST documentation, but I'm finding it challenging to configure the secure boot correctly.

Here are some specific points where I need help:

  1. How do I generate and program the required keys?
  2. Is there a recommended way to test the secure boot process?
  3. Any common pitfalls to avoid during configuration?

If anyone has experience with secure boot on STM32MP13 or can provide guidance or resources, it would be greatly appreciated!

Thank you for your time and support.

Best regards,
Hardin Jenne

1 REPLY 1