Skip to main content
JPabl.1
Associate III
November 13, 2024
Solved

How to find the custom recipe created in yocto inside st-image-qt

  • November 13, 2024
  • 3 replies
  • 1651 views

I created a st-image-qt image using the STM32MP Distribution package and X-LINUX-QT add-on for the STM32MP157F-DK2 board.

I could flash this image using the dd command in Linux and my target board is running correctly.

On the other side, I created a qt quick app using qt 6.7.3(which I could test ok using qt creator) and now I need to add this qt app in my st-image-qt image. I can bitbake this custom recipe doing "bitbake mygui"

I created the custom layer and a custom recipe and added this custom layer to my bblayers. Then, I built the image again with this custom recipe and it worked ok.

The problem is that I'm expecting to find this qt app inside my bin directory, but I can't see it.

 

SUMMARY = "This is the GUI for Hespect Software medical device"
DESCRIPTION = "Recipe created by bitbake-layers"
LICENSE = "CLOSED"
SECTION = "Mysection"

DEPENDS += " qtbase \
 qtdeclarative-native \
 qtdeclarative \
 qtquick3d \
 qtcharts"
 
RDEPENDS_${PN} += "qtwayland"

EXTRA_OECMAKE += "-DCMAKE_PREFIX_PATH=${STAGING_DIR_HOST}${prefix}"

SRC_URI += "file://main.cpp"
SRC_URI += "file://CMakeLists.txt"
SRC_URI += "file://CMakeLists.txt.user"
SRC_URI += "file://Backendsensors.h"
SRC_URI += "file://Backendsensors.cpp"
SRC_URI += "file://brushfactory.h"
SRC_URI += "file://brushfactory.cpp"
SRC_URI += "file://Main.qml"

# Add SVG images from the assets/images folder
SRC_URI += "file://assets/images/battery-full.svg"
SRC_URI += "file://assets/images/battery-mid.svg"
SRC_URI += "file://assets/images/rss-low.svg"
SRC_URI += "file://assets/images/signal-full.svg"
SRC_URI += "file://assets/images/signal-mid.svg"
SRC_URI += "file://assets/images/battery-low.svg"
SRC_URI += "file://assets/images/rss-full.svg"
SRC_URI += "file://assets/images/rss-mid.svg"
SRC_URI += "file://assets/images/signal-low.svg"

 
S = "${WORKDIR}/mygui"

do_install () {
 install -d ${D}${bindir}
 install -m 0775 mygui ${D}${bindir}/
}

FILES_${PN} += "${bindir}/mygui"

inherit cmake_qt5

 

In my local conf file I added: IMAGE_INSTALL_APPEND += "mygui"

This topic has been closed for replies.
Best answer by JPabl.1

The problem was in the syntax. Space at the beginning, and no space at the end works correctly 

 

IMAGE_INSTALL:append = " mygui" 

 

3 replies

Eldam
Senior
November 14, 2024

yop yop,

u should have a look at:

https://www.blaess.fr/christophe/yocto-lab/sequence-III-1/index.html

its written in french, quite easy language!

look a part :

Intégration de scripts shells

 

and from ure side:

 

IMAGE_INSTALL_APPEND += "mygui"

IMAGE_INSTALL_APPEND += " mygui" (note the space)

 

hope it helps!

 

JPabl.1
JPabl.1AuthorBest answer
Associate III
November 17, 2024

The problem was in the syntax. Space at the beginning, and no space at the end works correctly 

 

IMAGE_INSTALL:append = " mygui" 

 

JPabl.1
JPabl.1Author
Associate III
November 16, 2024

I added IMAGE_INSTALL_APPEND += " gui" and compiled the image. When flashing the board I look for /usr/bin/gui but can't find anything. The closes thing I could find is usr/share/examples/gui but it has a "rasterwindow" file, so I think it didn't work

 

Note: I tried building fresh so I'm using gui instead of mygui