cancel
Showing results for 
Search instead for 
Did you mean: 

How to display splash screen on HDMI monitor?

La1
Associate III

Hi i want to display splash screen on HDMI monitor instead of DSI monitor of STM32MP157C-DK2. I know that it has something to do with U-Boot configuration, but i can't find right options to enable this feature. I would be grateful if somebody could help me.

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @La​ 

Guess this page might help https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi, thanks for answer, but i have not found useful information there. They only say that "The U-Boot graphical console ("ST life.augmented" picture) is never displayed on the HDMI monitor. This console is displayed on the DSI display (if any on the board).", but i assume, that it is only on default starter package and it can be changed using developer or distribution package. On page https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_description they say that U-Boot supports "Display: LCD, HDMI, BMP for splashcreen", so i think it should be possible.