2022-10-10 9:32 PM
I am having difficulties using built-in ST-Link debugger on STM32MP157D-DK1 Discovery Kit. I am using the latest version of the STM32CubeIDE, Version: 1.10.1. Upon connecting the debugger it asked for FW upgrade on the ST-Link which I accepted and it completed the FW upgrade successfully.
GDB Connection: Autostart local GDB server
Debugger Load Mode: thru JTAG/SWD Link
I have configure the debug probe to be OpenOCD
Connection setup: SWD
Dropped the clock to 4, and 1.8 none worked.
Here is the log for the debugger:
Open On-Chip Debugger 0.11.0+dev-00449-g53fa0f7 (2022-06-09-09:42)
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J40M27 (API v2) VID:PID 0483:3752
Info : Target voltage: 3.245293
Info : clock speed 125 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP157DACx.cm4: Cortex-M4 r0p1 processor detected
Info : STM32MP157DACx.cm4: target has 6 breakpoints, 4 watchpoints
Info : STM32MP157DACx.cm4: external reset detected
Info : STM32MP157DACx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157DACx.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for STM32MP157DACx.cpu0 on 3334
Info : Listening on port 3334 for gdb connections
Info : starting gdb server for STM32MP157DACx.cm4 on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP157DACx.cm4:
Info : New GDB Connection: 1, Target STM32MP157DACx.cm4, state: reset
Warn : GDB connection 1 on target STM32MP157DACx.cm4 not halted
Warn : negative reply, retrying
Warn : negative reply, retrying
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : Deferring arp_examine of STM32MP157DACx.cm4
Info : Use arp_examine command to examine it manually!
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP157DACx.cm4: Cortex-M4 r0p1 processor detected
Info : STM32MP157DACx.cm4: target has 6 breakpoints, 4 watchpoints
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1828 ms). Workaround: increase "set remotetimeout" in GDB
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1831 ms). Workaround: increase "set remotetimeout" in GDB
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1835 ms). Workaround: increase "set remotetimeout" in GDB
Warn : target STM32MP157DACx.cm4 is not halted (add breakpoint)
Error: can't add breakpoint: target running
2022-10-12 6:01 AM
Hi @Saeed ,
I encourage you to check the following wiki pages
https://wiki.st.com/stm32mpu/wiki/Getting_started
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'