2020-12-04 03:23 AM
Hello Everyone
I am using the README.HOW_TO.txt file to install the kernel. IN section 3 it is stated that I must apply some patches:
1-Section 3 patch application
if there is some patch, please apply it on source code
$> for p in `ls -1 *.patch`; sudo do patch -p1 < $p; done
mehdi@LAPTOP-CP6QP7G9:~/DevPack/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0$ for p in *.patch; do sudo patch --strip=1 < $p; done
can't find file to patch at input line 16
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|From 4556074b66971918536ed27d52f5f4f6337f0646 Mon Sep 17 00:00:00 2001
|From: Lionel VITTE <lionel.vitte@st.com>
|Date: Mon, 5 Oct 2020 13:19:40 +0200
|Subject: [PATCH 01/22] ARM-stm32mp1-r2-rc8-MACHINE
|
|---
| arch/arm/kernel/time.c | 2 ++
| arch/arm/mach-stm32/Kconfig | 1 +
| arch/arm/mach-stm32/board-dt.c | 2 ++
| 3 files changed, 5 insertions(+)
|
|diff --git a/arch/arm/kernel/time.c b/arch/arm/kernel/time.c
|index b996b2cf07038..dddc7ebf4db44 100644
|--- a/arch/arm/kernel/time.c
|+++ b/arch/arm/kernel/time.c
--------------------------
File to patch: 0018-ARM-stm32mp1-r2-SOUND.patch
patching file 0018-ARM-stm32mp1-r2-SOUND.patch
Hunk #1 FAILED at 9.
Hunk #2 FAILED at 107.
2 out of 2 hunks FAILED -- saving rejects to file 0018-ARM-stm32mp1-r2-SOUND.patch.rej
can't find file to patch at input line 35
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/arch/arm/mach-stm32/Kconfig b/arch/arm/mach-stm32/Kconfig
|index 57699bd8f1075..8f9fd1da9ea05 100644
|--- a/arch/arm/mach-stm32/Kconfig
|+++ b/arch/arm/mach-stm32/Kconfig
--------------------------
How do I do that ? Can you give me an example?
I am working in the following directory which contains patches that I will link in a picture.
Directory :
~/DevPack/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0
----------------------------------------------------------------------------------------------------------------------------------
2- section 4: have a better management of the kernel
Now coming to section 4 of the .txt file. It is written that I have to:
test -d .git || git init . && git add . && git commit -m "new kernel" && git gc
But I get the following error even with sudo:
/home/mehdi/DevPack/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/.git: Permission denied
Best regards :grinning_face:
Solved! Go to Solution.
2020-12-07 05:57 AM
Hi @SigmaPrime ,
Are you using a git repository now ?
You have to choose one way of working : either from web source package using patch -p1 or either using git repository and git am $p
Can you please clarify ?
Olivier
2020-12-04 05:16 AM
Hi @SigmaPrime ,
You need to be in subdirectory linux-5.4.56 ( where are located source on which patch applied and call following command :
$>for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
Olivier
2020-12-04 06:10 AM
What an error of mine... I was confused when I read directory to kernel source code.
Works fine thanks
2020-12-07 05:52 AM
Hello
in the 4th step I have to
for p in `ls -1 <path to patch>/*.patch`; do git am $p; done
What is meant by <path to patch> ?
when I am in linux-5.4.56 and do
for p in `ls -1 ../*.patch`; do git am $p; done
I get this
Applying: ARM-stm32mp1-r2-rc8-MACHINE
warning: arch/arm/kernel/time.c has type 100755, expected 100644
error: patch failed: arch/arm/kernel/time.c:9
error: arch/arm/kernel/time.c: patch does not apply
warning: arch/arm/mach-stm32/Kconfig has type 100755, expected 100644
error: patch failed: arch/arm/mach-stm32/Kconfig:46
error: arch/arm/mach-stm32/Kconfig: patch does not apply
warning: arch/arm/mach-stm32/board-dt.c has type 100755, expected 100644
error: patch failed: arch/arm/mach-stm32/board-dt.c:17
error: arch/arm/mach-stm32/board-dt.c: patch does not apply
Patch failed at 0001 ARM-stm32mp1-r2-rc8-MACHINE
Use 'git am --show-current-patch' to see the failed patch
When you have resolved this problem, run "git am --continue".
If you prefer to skip this patch, run "git am --skip" instead.
To restore the original branch and stop patching, run "git am --abort".
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
fatal: previous rebase directory .git/rebase-apply still exists but mbox given.
2020-12-07 05:57 AM
Hi @SigmaPrime ,
Are you using a git repository now ?
You have to choose one way of working : either from web source package using patch -p1 or either using git repository and git am $p
Can you please clarify ?
Olivier
2020-12-07 05:59 AM
Oh ! then I have to skip step 4.1 and 4.2 and go to 5 cause I already did step 3. Is that right ?
2020-12-07 06:03 AM
Yes that's it ! :smiling_face_with_smiling_eyes:
2020-12-07 06:04 AM
Also is there a difference between <directory to kernel source code> (the linux-5.4.56) and <directory to kernel standard source code>
2020-12-07 06:07 AM
No it point to the same directory linux-5.4.56.
Olivier
2020-12-07 06:21 AM
Solved