2024-11-19 2:43 PM
I created a custom linux image for this target using the distribution package + x-linux-qt and the image "st-image-qt". This image is working correctly on my target.
Now, I want to add UART5 and UART4 to receive data over those 2 serial ports. As far as I understand, I need to add something like this in the DTS
&usart4 {
pinctrl-names = "default", "sleep", "idle";/* pin configurations definition */
pinctrl-0 = <&usart4_pins_a>; /* default pin configuration selection */
pinctrl-1 = <&usart4_sleep_pins_a>; /* sleep pin configuration selection */
pinctrl-2 = <&usart4_idle_pins_a>; /* idle pin configuration selection */
status = "okay";
};
and something like this in the DTSI
usart3_pins_a: usart3-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 10, AF7)>, /* USART3_TX */
<STM32_PINMUX('G', 8, AF8)>; /* USART3_RTS */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
pins2 {
pinmux = <STM32_PINMUX('B', 12, AF8)>, /* USART3_RX */
<STM32_PINMUX('I', 10, AF8)>; /* USART3_CTS_NSS */
bias-disable;
};
};
usart3_idle_pins_a: usart3-idle-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 10, ANALOG)>, /* USART3_TX */
<STM32_PINMUX('G', 8, ANALOG)>, /* USART3_RTS */
<STM32_PINMUX('I', 10, ANALOG)>; /* USART3_CTS_NSS */
};
pins2 {
pinmux = <STM32_PINMUX('B', 12, AF8)>; /* USART3_RX */
bias-disable;
};
};
usart3_sleep_pins_a: usart3-sleep-0 {
pins {
pinmux = <STM32_PINMUX('B', 10, ANALOG)>, /* USART3_TX */
<STM32_PINMUX('G', 8, ANALOG)>, /* USART3_RTS */
<STM32_PINMUX('I', 10, ANALOG)>, /* USART3_CTS_NSS */
<STM32_PINMUX('B', 12, ANALOG)>; /* USART3_RX */
};
};
My question is, should I override these files in my tmp-glibc/work-shared folder? or do I need to create new ones in my custom layer?
There's so much different paths and different documentation that I don't really understand which one should I be using
2024-12-03 6:00 AM
Hi, I am also stuck with the same thing, please let me know if you find solution