cancel
Showing results for 
Search instead for 
Did you mean: 

How can I get the MMC timing spec higher than sd high-speed?

Hello,

I am having difficulties with the MMC bus and the external SDIO wifi module. We are using the wifi module jody-w263 from U-blox with the OSD32MP1, and the communication with the module works, but it is quite slow. The wifi module is capable of SDR 104 and DDR50 communication speeds, but I add the support to the DTS, the communication is broken and the device returns the -110 while initializing.

How can I add support for higher speeds?

I attach the working dts, dmesg, ios and caps, and relevant schematic.

Any suggestion will be appreciated.

Best regards,

Tomáš.

This discussion is locked. Please start a new topic to ask your question.
75 REPLIES 75

Hello Bernard,

I have applied all three provided patches but the still no change. The boot log is attached.

Bernard PUEL
ST Employee

Hello Tomas,

I see this trace:

[  3.273770] mmci-pl18x 48004000.sdmmc: mmc_regulator_set_vqmmc: found vmmc voltage range of 3300000-3400000uV

Are you sure you have "vqmmc-supply = <&v1v8_ldo1>;" in your devicetree ?

Hello,

yes, this line is there. I am attaching the dts file, that is in the yocto build directory (i.e. <yocto_build>/tmp-glibc/work/stm32mp157c_tevogs_v3_mx-ostl-linux-gnueabi/linux-stm32mp/5.4.56-r0/linux-5.4.56/arch/arm/). I also attach the decompiled dts that I took from the build dir and the dtb itself so you can check it. The v1v8_ldo1 regulator has the phandle number 0x2b and the same value is referenced in the vqmmc-supply of the sdmmc@48004000 node.

p.s.: in the decompiled file I had found the max-frequency is 120 Mhz, so I guess it is the default value, if not specified in the dts.

Bernard PUEL
ST Employee

Hello Tomas,

Thanks for the information.

kindly apply this new debug patch on top of all the rest and send me back the log.

I think we are not so far be we are still missing one trick ...

Hi Bernard,

glad to hear that and thank you for your support.

The log is attached.

Bernard PUEL
ST Employee

new tentative patch + more traces in case of failure, please apply the 2 patches on top of previous ones.

Bernard PUEL
ST Employee
 

The boot log.

Bernard PUEL
ST Employee

new debug trace. Thanks for your patience.

Hello Bernard,

I am sending the log with the last patch.