Senior
August 2, 2021
Solved
How can I get the MMC timing spec higher than sd high-speed?
- August 2, 2021
- 75 replies
- 30401 views
Hello,
I am having difficulties with the MMC bus and the external SDIO wifi module. We are using the wifi module jody-w263 from U-blox with the OSD32MP1, and the communication with the module works, but it is quite slow. The wifi module is capable of SDR 104 and DDR50 communication speeds, but I add the support to the DTS, the communication is broken and the device returns the -110 while initializing.
How can I add support for higher speeds?
I attach the working dts, dmesg, ios and caps, and relevant schematic.
Any suggestion will be appreciated.
Best regards,
Tomáš.