2022-11-16 1:17 AM
2022-11-16 1:31 AM
Hi @rahuj.1
USBH could use port0(USB_DP1/DM1 pins), this is the case on our EV1 and DK2 boards, and in addition also on port1 (USB_DP2/DM2 pins).
Please refer to https://wiki.st.com/stm32mpu/wiki/USBH_device_tree_configuration#DT_configuration_when_using_port0
or
Note that OTG cannot be 'routed' on port0 (USB_DP1/DM1 pins). OTG high-speed is only possible on port1 (USB_DP2/USBDM2 pins) which is mandatory for flashload (e.g. with CubeProgrammer)
For possible HW choices around USB, please refer to AN5031.
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-11-27 7:58 PM
thanks @PatrickF . this was really helpful
2022-11-29 11:40 PM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'