cancel
Showing results for 
Search instead for 
Did you mean: 

Hi Is there a ST controller/processor that can support interface to a 8Mpixel (CSI) camera? I need a LOW COST solution for transmitting, in a very low rate, pictures taken from a 8Mpixel camera. Thanks!

Aharon1
Associate II
 
2 REPLIES 2
TDK
Guru

The STM32MP series can communicate with CSI, but I don't think any STM32 MCUs can.

https://www.st.com/resource/en/application_note/dm00693021-stm32mp1-series-interfacing-with-a-mipi-csi2-camera-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for your reply,

I understand that they can not interface it directly but require the STMIPID02, It seems that between STM32MP1 and STMIPID02 I arrive almost at 10euros, close to the price of Raspberry Pi Zero WH, is there another cheaper way to do it?

*I don't even need to process the image, just communicate it further

Best regards