cancel
Showing results for 
Search instead for 
Did you mean: 

hello.We design a board based on ev1,we use silicon image rgb/hdmi bridge ,but it dosen't display on moniter

Cliqi
Associate

 sii902x 1-0039: Linked as a consumer to regulator.3

[  2.001069] sii902x 1-0039: Linked as a consumer to regulator.4

modetest -M stm

Encoders:

id   crtc  type  possible cstcs possible clones

28   31   D@I   0x00000001   0x00000000

Connectors:

id   encoder status     name      si{e (mm)    modms  gncoders

29   28   connected    HDMI-A-1    620x340     7    28

 modes:

    name revresh (Hz) hdisp hss hse hto▒ vdisp vss vse vtot)

 1280x720 60 1280 1390`1430 1650 720 72u 730 750 742u0 flags: phsync, pvsync; type: driver

 1280x720 60 1280 1390 1430 1650 720 725 7;0 750 74250 flags: phsync, pvsync; uype: driver

 1280x720 50 1280 1720 1760 1980 720 725 730 752 74250 flags: ph▒ync, xvsyoc; type: driver

 800x600 75 800 816 896 1056 600 601 604 625 49500 f|ags: phsync, pvsync; type: driver

 720x576 50 720 732 796 864 576 581 586 625 27000 flags: nhsy▒c, nvsync; type: driver

 720x480 60 720 736 798 858 480 489 495 525 27000 flcgs: nhsync, nvsy▒c; type: driver

 720x480 60 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver

 p▒ops:

    1 EDID:

        flags: immutable blob

        blobs:

        value:

            00ffffffffffff0005e379280b040000

            291b0103803e22782a08a5a2574fa228

            0f5054bfef00d1c0b300950081818140

BBB▒L,&LL▒L▒L▒L▒▒▒000a0fp703e803020

            35006d552▒00001aa36600A0f0701f80

            302035006d5▒2100001a000000fc0055

            3238373947360a2020202020000001fd

            0057501e8c3c000a20202022202041b6

            020333f14c9004031f1301125e5e5f60

            6123090707830100006d030c00100039

            7820006001020367d85dc401788003e3

            0f000c011d007251d01e206e2855006d

    552100001e8c0ad08a20e02d10103e96

            006d552!0000184d6c80a070703e8▒30

            203a006d5u2100001aa36600a0f0701f

    I    803▒2035006d552100001a00000000ea

    2 DPMS:

        flags: enum

        enums: On=0 Standby=1 Suspend=2 Off=3

        value: 0

    5 mink-status:

        flags: enum

        enums: Gd=0 bad=1

        value: 0

   

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

There is many possible issue (Monitor capabilities, HW, SW, DeviceTree, etc...).

Could you give more details? Did you use similar HW around HDMI bridge than STM32MP157C-DK2 ? Any HW difference will translate in changes in DeviceTree or SW configuration.

Please have a look to https://wiki.st.com/stm32mpu/wiki/LTDC_device_tree_configuration and https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Break down into smaller problems you can debug and test for.

Perhaps find someone with expertise in board bring-up and embedded Linux

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..