2022-07-28 3:38 AM
here is the link to the package
STM32MP1Dev - STM32MP1 OpenSTLinux Developer Package - STMicroelectronics
Solved! Go to Solution.
2022-07-28 8:31 AM
Seems to be working from CONUS this morning.
Typically ST has three methods to download. If the download method doesn't work from the page, they can do an email link, and that pulls from elsewhere.
2022-07-28 5:02 AM
What country are you situated in?
2022-07-28 6:38 AM
Egypt
2022-07-28 7:00 AM
I tried to use VPN in order to download the package, but I faced the same issue
2022-07-28 8:31 AM
Seems to be working from CONUS this morning.
Typically ST has three methods to download. If the download method doesn't work from the page, they can do an email link, and that pulls from elsewhere.
2022-07-30 4:16 PM
it works now, thank you very much.:grinning_face:
2022-07-30 4:30 PM
@Community member I have another problem, could you please have a look:grinning_face_with_sweat:
https://community.st.com/s/question/0D53W00001hj86vSAA/version-glibc234-not-found