cancel
Showing results for 
Search instead for 
Did you mean: 

Ethernet not working in the DK2 board out of the box.

SKris
Associate III

We are new the MPUs and Linux. We received a new STM32MP157F-DK2 board, out of the box and boots up with the default binaries in the SD card.

However, we find that the ethernet is not working (the LD3 is blinking).

root@stm32mp1:~# ifconfig -a

eth0   Link encap:Ethernet HWaddr 00:80:E1:42:84:8F

     inet6 addr: fe80::280:e1ff:fe42:848f/64 Scope:Link

     UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1

     RX packets:819 errors:0 dropped:50 overruns:0 frame:0

     TX packets:50 errors:0 dropped:0 overruns:0 carrier:0

     collisions:0 txqueuelen:1000

     RX bytes:58744 (57.3 KiB) TX bytes:8502 (8.3 KiB)

     Interrupt:54 Base address:0xc000

lo    Link encap:Local Loopback

     inet addr:127.0.0.1 Mask:255.0.0.0

     inet6 addr: ::1/128 Scope:Host

     UP LOOPBACK RUNNING MTU:65536 Metric:1

     RX packets:184 errors:0 dropped:0 overruns:0 frame:0

     TX packets:184 errors:0 dropped:0 overruns:0 carrier:0

     collisions:0 txqueuelen:1000

     RX bytes:10720 (10.4 KiB) TX bytes:10720 (10.4 KiB)

usb0   Link encap:Ethernet HWaddr 0A:68:50:EF:AD:61

     UP BROADCAST MULTICAST MTU:1500 Metric:1

     RX packets:0 errors:0 dropped:0 overruns:0 frame:0

     TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

     collisions:0 txqueuelen:1000

     RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

wlan0   Link encap:Ethernet HWaddr C4:AC:59:83:77:8F

     BROADCAST MULTICAST MTU:1500 Metric:1

     RX packets:0 errors:0 dropped:0 overruns:0 frame:0

     TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

     collisions:0 txqueuelen:1000

     RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

I have copy-pasted only the ethernet logs below which show that the the link is Up.

root@stm32mp1:~# dmesg | grep eth

[  0.000000] psci: probing for conduit method from DT.

[  1.468806] stm32-dwmac 5800a000.ethernet: PTP uses main clock

[  1.473249] stm32-dwmac 5800a000.ethernet: no reset control found

[  1.479308] stm32-dwmac 5800a000.ethernet: No phy clock provided...

[  1.502019] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42

[  1.507531] stm32-dwmac 5800a000.ethernet:  DWMAC4/5

[  1.512539] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported

[  1.519793] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported

[  1.527131] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported

[  1.533993] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported

[  1.540237] stm32-dwmac 5800a000.ethernet: TSO supported

[  1.545565] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer

[  1.553394] stm32-dwmac 5800a000.ethernet: TSO feature enabled

[  1.588202] usbcore: registered new interface driver cdc_ether

[  2.048522] optee: probing for conduit method from DT.

[  8.029018] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found

[  8.056288] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported

[  8.072664] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock

[  8.089364] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

[  9.232265] using random self ethernet address

[  9.235675] using random host ethernet address

[  13.273126] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx

[  13.280228] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

We would like to determine it is a faulty board or if we are missing something. Any help is much appreciated.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
SKris
Associate III

Hi Patrick,

Thanks for the pointers.

The ethernet on the DK-2 board was working fine when connected to home network with proper IP address being assigned.

Guess it was some firewall at office preventing it, which was resolved by the system admin and it now works at office too.

Thanks.

View solution in original post

2 REPLIES 2
PatrickF
ST Employee

Hi,

Not LAN expert, but seems you eth0 is UP and RUNNING (LD3 is normal, should blink on Gigabit network activity).

Seems that your network DHCP has only assigned an IPv6 address to your board, which might not be what you wanted.

See this similar post https://community.st.com/s/question/0D50X0000B31mTmSQI/stm32mp157dk2-not-connecting-to-ethernet

Btw, I think that out of the box, the code provided in the flash is not the latest Ecosystem V3. A good exercise would be to reflash your board (see https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image). Note that Flashing starter package could also be done with CubeProgrammer under W10 (no need of Linux at this point).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SKris
Associate III

Hi Patrick,

Thanks for the pointers.

The ethernet on the DK-2 board was working fine when connected to home network with proper IP address being assigned.

Guess it was some firewall at office preventing it, which was resolved by the system admin and it now works at office too.

Thanks.