cancel
Showing results for 
Search instead for 
Did you mean: 

Error message inquiries and display problems

LeeJaewon
Associate II

Hello, I developed a custom board with a pinmap based on stm32mp157f - dk2.

I think if you match the pinmap and use the start package, lcd and other features will work.

I re-created the sd card according to that advice, and I also rebooted it, but the same thing is happening.

What should I do?

LeeJaewon_0-1728536466946.png

History: https://community.st.com/t5/stm32-mpus-products/error-message-inquiries-and-display-problems/m-p/714459#M11850

https://community.st.com/t5/stm32-mpus-boards-and-hardware/check-error-code-for-uart4/td-p/700161

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @LeeJaewon 

"devil is in the details".

I think you should check what you made different versus stm32mp157F-dk2 board. Unless you are really insightful of the system, even very small board change could lead to a blocking point.

Are you using exactly same STPMIC1 and supply usage ? USB Type-C supply with ADC connections ? Ethernet PHY, etc...

Custom board is usually meaning custom device tree and need to build complete image.

STM32MP157F-DK2 image are not build with other boards binary compatibility in mind.

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Hi @LeeJaewon 

"devil is in the details".

I think you should check what you made different versus stm32mp157F-dk2 board. Unless you are really insightful of the system, even very small board change could lead to a blocking point.

Are you using exactly same STPMIC1 and supply usage ? USB Type-C supply with ADC connections ? Ethernet PHY, etc...

Custom board is usually meaning custom device tree and need to build complete image.

STM32MP157F-DK2 image are not build with other boards binary compatibility in mind.

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.