2020-11-12 2:39 PM
Hello,
I tried to apply the step by step "Modify, rebuild and reload the Linux® kernel" form wiki.st .
Everything works fine from the first step of the "Getting started " until i uncoutered the error bellow.
Unfortunately i am a complete beginner on these tools and don't understand whats happen.
Thank you by advance for any help.
@PC:~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.31-r0/linux-5.4.31$ make ARCH=arm multi_v7_defconfig "fragment*.config"
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
HOSTCC scripts/kconfig/confdata.o
HOSTCC scripts/kconfig/expr.o
LEX scripts/kconfig/lexer.lex.c
/bin/sh: 1: flex: not found
scripts/Makefile.host:9: recipe for target 'scripts/kconfig/lexer.lex.c' failed
make[2]: *** [scripts/kconfig/lexer.lex.c] Error 127
Makefile:567: recipe for target 'multi_v7_defconfig' failed
make[1]: *** [multi_v7_defconfig] Error 2
Makefile:326: recipe for target '__build_one_by_one' failed
make: *** [__build_one_by_one] Error 2
Solved! Go to Solution.
2020-11-12 11:51 PM
Hi @Sisyphus38
Open a new shell and source again the SDK.
If one of my comments answer your need, please mark it "Best answer"
Olivier
2020-11-12 3:49 PM
Hello,
A little web search solves the issue. I needed to install two extra packages with
-apt-get install flex
-apt-get install bison
For information, my computer was running i Ubuntu 18.04 fresh install.
Regards
2020-11-12 3:55 PM
Next issue......
when running make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
.....
.......
WRAP arch/arm/include/generated/asm/trace_clock.h
WRAP arch/arm/include/generated/asm/simd.h
UPD include/config/kernel.release
UPD include/generated/uapi/linux/version.h
UPD include/generated/utsrelease.h
SYSNR arch/arm/include/generated/asm/unistd-nr.h
GEN arch/arm/include/generated/asm/mach-types.h
SYSTBL arch/arm/include/generated/calls-oabi.S
SYSTBL arch/arm/include/generated/calls-eabi.S
CC scripts/mod/empty.o
gcc: error: unrecognized argument in option ‘-mabi=aapcs-linux’
gcc: note: valid arguments to ‘-mabi=’ are: ms sysv
gcc: error: unrecognized command line option ‘-mlittle-endian’; did you mean ‘-fconvert=little-endian’?
gcc: error: unrecognized command line option ‘-mfpu=vfp’; did you mean ‘-mcpu=’?
scripts/Makefile.build:265: recipe for target 'scripts/mod/empty.o' failed
make[1]: *** [scripts/mod/empty.o] Error 1
Makefile:1110: recipe for target 'prepare0' failed
make: *** [prepare0] Error 2
Thank you by advance for any help.
2020-11-12 4:15 PM
Some think completely broke my SDK install.
The "Hello World" does'nt compile any more.
$CC --version -> unknown command
echo $CROSS_COMPILE -> gives empty string.
I will reinstall the SDK and give you feedback.
Regards
2020-11-12 11:50 PM
Hi @Sisyphus38
Yes you have to proceed carefully to installation of all extra package as mentionned here :
https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Install_extra_packages
Olivier
2020-11-12 11:51 PM
Hi @Sisyphus38
Open a new shell and source again the SDK.
If one of my comments answer your need, please mark it "Best answer"
Olivier
2020-11-13 1:23 AM
Thank you Olivier for your
2020-11-13 1:38 AM
Hello Olivier,
You right. When I source again all env variables are retrieved and the "Hello world" compile again !
I launched make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040 and compiling is still proceeding .
Good signal !
Thank you again Olivier.
2021-01-14 12:01 PM
Hi @Sisyphus38 and @Community member How do you fix this problem; it has taken me more than three days now; I delete the whole Linux system from my virtual machine, and reinstall it again by following all steps outlined at the WIKI. But no success; I keep getting the same error
2021-01-15 5:02 AM
I have applied the process on an Ubuntu 18.04 fresh install.
All compilation module installed are those of the step by step Stm wiki . No one more.
Be aware that when you source the compiler, it's only available the currently opened linux shell.
All modules installed are in the exact version adviced in the wiki.
Be confident. The setup works well....
Back to you if some details come back to the mind.
Regards.