2019-08-29 07:19 AM
Hallo,
Im trying to flash an image (st-example-image-qt-openstlinux-eglfs-stm32mp1), bu it fails on partition 0x23
this is the output on Terminal:
giomate@giolaptop:~/Development/STM32/MP15/Distribution/openstlinux/build-openstlinuxeglfs-stm32mp1/tmp-glibc/deploy/images/stm32mp2/stm32mp1$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-example-image-qt/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv -log
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: /home/giomate/.STM32CubeProgrammer/trace.log
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000
SN : 0030002C3338510939303435
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: st-example-image-qt-openstlinux-eglfs-stm32mp1.ext4
File : st-example-image-qt-openstlinux-eglfs-stm32mp1.ext4
Size : 1086306 KBytes
Partition ID : 0x23
Download in Progress:
[=================================== ] 70%
Error: failed to download Segment[0]
Error: failed to download the File
Time elapsed during download operation: 00:14:00.737
Error: Download partition 0x23 failed
Error: TSV flashing service failed
I appeciate any comment or suggestions
Solved! Go to Solution.
2019-08-31 07:10 AM
Yeap, it was the sizes of the roofs partition
2019-08-29 11:35 PM
Probably linked to that issue (assigned size/offset in Flashlayout too small for your image) https://community.st.com/s/question/0D50X0000B7Ykl5SQC/getting-failure-while-compiling-qtwebkit-for-yocto
2019-08-31 07:10 AM
Yeap, it was the sizes of the roofs partition