2019-05-05 9:59 AM
Is the USB controller in MP chips same as in F7 (Tensilica) or compatible?
Does it support connection of devices thru a full speed hub?
Does it support OTG mode?
Thanks,
Pavel A.
Solved! Go to Solution.
2019-05-05 11:50 PM
In STM32MP1, there is two USB controllers with up to three ports with embedded PHY in total:
Notice that in STM32MP1, our SW delivery support USBH and OTG on Linux (Cortex-A7) only.
2019-05-05 11:50 PM
In STM32MP1, there is two USB controllers with up to three ports with embedded PHY in total:
Notice that in STM32MP1, our SW delivery support USBH and OTG on Linux (Cortex-A7) only.
2019-05-06 9:27 AM
Thank you, @PatrickF for the explanation.
-- pa