Associate II
March 12, 2019
Solved
STUSB1600 (USB Type-C) and USB OTG
- 8 replies
- 7351 views
I'm trying to understand how I can use a USB Type-C connector together with the STM32MP1 USB OTG peripheral.
So obviously I want to use the port in dual role configuration. I want to use the STUSB1600 for that because it takes care of the power source/sink control for me. But I do wonder how should I connect the OTG_ID pin (if at all) in the STM32MP1, should it be to the ATTACH pin of the STUSB1600? The eval and DK only use the micro connectors for OTG.
I have found AN4775 and figure 9 (attached) explains how to use Type-C with OTG, but I'm not sure if that applies with the STUSB1600 because it takes care of the CC pins for me.
So if someone could please help with figuring out dual role with Type-C connector, please.