2024-06-21 12:59 AM
LED blinking mode Console message Boot process
Twice | WARNING 500mA power supply detected Current too low, use a 3A power supply! | Continue and red LED stays ON |
3 times | WARNING 1500mA power supply detected Current too low, use a 3A power supply! | Continue and red LED stays ON |
forever | ERROR USB TYPE-C connection in unattached mode Check that USB TYPE-C cable is correctly plugged | stop |
forever | USB TYPE-C charger not compliant with USB specification | stop |
I confirm that my power supply supports 5V3A.
my log as follow:
Previous ADC measurements was not the one expected, retry in 20ms
********************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
*******************************************************
Solved! Go to Solution.
2024-06-21 8:15 AM
HI @tomcat
current which could be provided by the supply is one thing, but the current capabilities exposed to the USB Type-C as per the standard matters.
I think you are using a Type-A -> Type-C cable. Please try an USB Type-C charger.
Alternatively, there is way to disable this check in the device tree.
Regards
2024-06-21 8:15 AM
HI @tomcat
current which could be provided by the supply is one thing, but the current capabilities exposed to the USB Type-C as per the standard matters.
I think you are using a Type-A -> Type-C cable. Please try an USB Type-C charger.
Alternatively, there is way to disable this check in the device tree.
Regards
2024-06-23 7:28 AM
First of all, thank you for your reply!
I've tried using an USB Type-C charger, the result was the same.
--"Alternatively, there is way to disable this check in the device tree. "
--What can I do to disable this check in the device tree?
2024-06-23 11:16 PM
HI @tomcat
strange that an USB Type-C charger (with a Type-C <-> Type-C cable) does not work. There is probably some chargers not fully compliant with the standard (even if working with some phones, which could also use different way to detect capabilities like quick-charge).
To disable the check in the SW, see this post https://community.st.com/t5/stm32-mpus-boards-and-hardware/my-stm32mp157f-dk2-is-powered-by-5v-3a-psu-but-at-the-boot-up/m-p/211924/highlight/true#M472
It is related to STM32MP15-DK2, so definition is likely different as board is different, but it could probably help you.
Regards
2024-06-26 8:11 AM
I bought another power cord:
The previous log is no longer printed:
Previous ADC measurements was not the one expected, retry in 20ms
********************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
*******************************************************
The complete log is attached "log2024.06.26.txt".
Looking forward to your reply.
Regards