2020-03-27 2:37 AM
I’m trying to boot stm32mp157c-ev1 evaluation board with original device tree.
However, cannot boot the board when following steps
--Environment--
Host PC: Intel Core i7 3.6GHz / Ubuntu Ver16.04.6 LTS
STM32CubeMX: Version 5.6.0
OpenSTLinux: openstlinux-4.19-thud-mp1-20-02-19
--Steps--
1) Generate device tree sources by STM32CubeMX
2) Compile the device tree with Developer Package, and Get “kernel DTB�?, “u-boot.stm32�? and “TF-A.stm32�? files.
-according to following wiki page.
3) Flash “u-boot.stm32�? and “TF-A.stm32�? with following FlashLayout file.
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp157c-ev1-trusted.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp157c-ev1-trusted.stm32
P 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-xxxxxxx-mx-trusted.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-xxxxxxx-mx-trusted.stm32
P 0x06 ssbl Binary mmc0 0x00084400 u-boot.stm32
- 0x21 bootfs System mmc0 0x00284400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
- 0x22 vendorfs FileSystem mmc0 0x04284400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
- 0x23 rootfs FileSystem mmc0 0x05284400 st-image-weston-openstlinux-weston-stm32mp1.ext4
- 0x24 userfs FileSystem mmc0 0x33C84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
During this steps, There was no error.
However, when trying to boot the devices, following error message show and cannot boot the device.
PANIC at PC : 0x2ffd8000
Exeption mode=0x00000016 at: 0x2ffd8000
On the other hand, if I flash only “TF-A.stm32�? firstly, and then flash “u-boot.stm32�? individually, Booting the device was success.
Why do these two ways produce different results?
Would you be able to lend your expertise.
Best regards
Solved! Go to Solution.
2020-03-30 2:01 AM
Hi @HMasu.1
The fail boot log is not complete but only contain the PANIC message.
Anyway, the CubeMX project you sent CANNOT generate a bootable Device Tree.
CubeMX only generate "bootable" Device Tree for ST Board Project ( DK2 or EV1).
You have to carefully fill the USER SECTION according to your hardware taking EV1 Device tree as example.
Below wiki article to start :
https://wiki.st.com/stm32mpu/index.php/How_to_create_your_board_device_tree
Hope it help
Olivier
2020-03-27 3:44 AM
Hi @HMasu.1
Did you change anything in CubeMX compare to a default EV1 board project ?
Can you share both complete boot log : the one fail with PANIC and the one succeed after individual flash.
Thanks
Olivier
2020-03-29 6:17 PM
Hi OlivierG (ST Employee)
Thank you for your answer.
I have Changed many settings in Cube MX because my final goal is to operate my original board which STM32MP151CAA3 MPU is mounted on.
So, I share Cube MX project file and complete boot logs(success and fail).
Please check the attached files.
Thank you
H. Masuda
2020-03-30 2:01 AM
Hi @HMasu.1
The fail boot log is not complete but only contain the PANIC message.
Anyway, the CubeMX project you sent CANNOT generate a bootable Device Tree.
CubeMX only generate "bootable" Device Tree for ST Board Project ( DK2 or EV1).
You have to carefully fill the USER SECTION according to your hardware taking EV1 Device tree as example.
Below wiki article to start :
https://wiki.st.com/stm32mpu/index.php/How_to_create_your_board_device_tree
Hope it help
Olivier
2020-03-30 5:04 PM
Hi @Community member
Thank you for your answer.
Sorry, I don't know how to get complete boot log file.
Previous log text files attached this thread are all message that console shows.
>CubeMX only generate "bootable" Device Tree for ST Board Project ( DK2 or EV1).
>You have to carefully fill the USER SECTION according to your hardware taking EV1 Device tree as example.
Thank you for sharing the valuable information. I understand what is missing in my steps.
I will fill the User Section referring to the EV1 device tree..
Thank you for your kind support.
H.Masuda
2020-03-31 1:33 AM
Hi @Community member
Please let me ask again.
I tried to fill the User Section in device trees referring to the EV1 device tree.
However, the same boot error is displayed as before.
What could be the cause of the error?
Or, what should I try to get more information?
I share Cube MX project file and device tree source files(one is a original file from CubeMX, the other is a modified in user section) and display's capture when boot error occurs.
Please check the attached files.
Would you be able to lend your expertise.
Best regards
H. Masuda