cancel
Showing results for 
Search instead for 
Did you mean: 

Can't write the Stm32mp1 boot device by STM32CubeProgrammer

WHe.1
Associate II

Hello, I use the STM32CubeProgrammer to write Stm32mp157c board boot TF card. But it fail. How can I fix this problem?

0693W00000QMSPqQAP.png

1 REPLY 1
PatrickF
ST Employee

Hi @WHe.1​ 

looking at your TSV, you are using an old ecosystem (v2.1 likely) with an STM32MP157C-EV1 board.

Which version of STMCubeProg are you using ?

I tested to load en EV1 board with CubeProg v2.11 on W10 without issue.

Maybe worth to get console log output (available on STLINK VCP comm port).

Anyway, I recommend you to switch to latest ecosystem (V4.0) together with latest STM32CubeProg (v2.11)

some guidelines could be found on wiki

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.