2024-04-18 2:26 PM
I'm buildning my own computer by using STM32MP151AAC3.
I'm going to draw lines for the HDMI connector. I have one question: Can I transfer sound via the HDMI cable? For example if I run OpenSTLinux onto the STM32MP151AAC3 processor, and then I connect the HDMI cable and I can see the screen. Will I be able to hear sound too if I surf into Youtube?
Solved! Go to Solution.
2024-10-26 11:23 AM - edited 2024-10-26 11:25 AM
Hi @PatrickF
Note! What you are refering to is not the HDMI PHY.
You refering to another IC chip.
The linux kernel does not support sii9022A without MCLK.
I get these debug messages from sii902x.c https://github.com/torvalds/linux/blob/master/drivers/gpu/drm/bridge/sii902x.c because my device requries MCLK. I have not routed that track from my MCU to the PHY. So sound won't work for the moment until sii902x.c supports PLL as a clock instead of only MCLK.
if (daifmt->bit_clk_provider || daifmt->frame_clk_provider) {
dev_dbg(dev, "%s: I2S clock provider mode not supported\n", __func__); <--------------------------
return -EINVAL;
}
switch (daifmt->fmt) {
case HDMI_I2S:
i2s_config_reg |= SII902X_TPI_I2S_FIRST_BIT_SHIFT_YES |
SII902X_TPI_I2S_SD_JUSTIFY_LEFT;
break;
case HDMI_RIGHT_J:
i2s_config_reg |= SII902X_TPI_I2S_SD_JUSTIFY_RIGHT;
break;
case HDMI_LEFT_J:
i2s_config_reg |= SII902X_TPI_I2S_SD_JUSTIFY_LEFT;
break;
default:
dev_dbg(dev, "%s: Unsupported i2s format %u\n", __func__, daifmt->fmt); <--------------------------------
return -EINVAL;
}
The device tree requries the mclk.
https://www.kernel.org/doc/Documentation/devicetree/bindings/display/bridge/sil%2Csii9022.yaml
# SPDX-License-Identifier: (GPL-2.0-only OR BSD-2-Clause)
%YAML 1.2
---
$id: http://devicetree.org/schemas/display/bridge/sil,sii9022.yaml#
$schema: http://devicetree.org/meta-schemas/core.yaml#
title: Silicon Image sii902x HDMI bridge
maintainers:
- Boris Brezillon <bbrezillon@kernel.org>
properties:
compatible:
oneOf:
- items:
- enum:
- sil,sii9022-cpi # CEC Programming Interface
- sil,sii9022-tpi # Transmitter Programming Interface
- const: sil,sii9022
- const: sil,sii9022
reg:
maxItems: 1
interrupts:
maxItems: 1
description: Interrupt line used to inform the host about hotplug events.
reset-gpios:
maxItems: 1
iovcc-supply:
description: I/O Supply Voltage (1.8V or 3.3V)
cvcc12-supply:
description: Digital Core Supply Voltage (1.2V)
'#sound-dai-cells':
enum: [ 0, 1 ]
description: |
<0> if only I2S or S/PDIF pin is wired,
<1> if both are wired.
HDMI audio is configured only if this property is found.
If HDMI audio is configured, the sii902x device becomes an I2S and/or
S/PDIF audio codec component (e.g. a digital audio sink), that can be
used in configuring full audio devices with simple-card or
audio-graph-card bindings. See their binding documents on how to describe
the way the
sii902x device is connected to the rest of the audio system:
Documentation/devicetree/bindings/sound/simple-card.yaml
Documentation/devicetree/bindings/sound/audio-graph-card.yaml
Note: In case of the audio-graph-card binding the used port index should
be 3.
sil,i2s-data-lanes:
$ref: /schemas/types.yaml#/definitions/uint32-array
minItems: 1
maxItems: 4
uniqueItems: true
items:
enum: [ 0, 1, 2, 3 ]
description:
Each integer indicates which I2S pin is connected to which audio FIFO.
The first integer selects the I2S audio pin for the first audio FIFO#0
(HDMI channels 1&2), the second for FIFO#1 (HDMI channels 3&4), and so
on. There are 4 FIFOs and 4 I2S pins (SD0 - SD3). Any I2S pin can be
connected to any FIFO, but there can be no gaps. E.g. an I2S pin must be
mapped to FIFO#0 and FIFO#1 before mapping a channel to FIFO#2. The
default value is <0>, describing SD0 pin being routed to HDMI audio
FIFO#0.
clocks:
maxItems: 1
description: MCLK input. MCLK can be used to produce HDMI audio CTS values.
clock-names:
const: mclk
ports:
$ref: /schemas/graph.yaml#/properties/ports
properties:
port@0:
$ref: /schemas/graph.yaml#/properties/port
description: Parallel RGB input port
port@1:
$ref: /schemas/graph.yaml#/properties/port
description: HDMI output port
port@3:
$ref: /schemas/graph.yaml#/properties/port
description: Sound input port
required:
- compatible
- reg
additionalProperties: false
examples:
- |
i2c {
#address-cells = <1>;
#size-cells = <0>;
hdmi-bridge@39 {
compatible = "sil,sii9022";
reg = <0x39>;
reset-gpios = <&pioA 1 0>;
iovcc-supply = <&v3v3_hdmi>;
cvcc12-supply = <&v1v2_hdmi>;
#sound-dai-cells = <0>;
sil,i2s-data-lanes = < 0 1 2 >;
clocks = <&mclk>;
clock-names = "mclk";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
bridge_in: endpoint {
remote-endpoint = <&dc_out>;
};
};
};
};
};
2024-10-27 3:39 PM - edited 2024-10-27 3:56 PM
Hi @PatrickF
I have updated my DT.
Instead of ASoC Audio Graph Card, I'm using Simple Sound Card instead. It seems like I can get a hdmi-audio-codec and ha i2s-hifi...I don't know what they are doing.
/ {
hdmi:connector{
compatible = "hdmi-connector";
#sound-dai-cells = <0>;
label = "hdmi";
type = "a";
port{
hdmi_connector_in:endpoint{
remote-endpoint = <&sii9022_out>;
};
hdmi_audio_out:endpoit{
remote-endpoint= <&sii9022_tx_endpoint>;
};
};
};
sound {
compatible = "simple-audio-card";
simple-audio-card,name = "SII9022A HDMI";
simple-audio-card,format = "i2s";
simple-audio-card,widgets = "Speaker", "External Speaker";
simple-audio-card,routing = "External Speaker", "LINE_OUT";
simple-audio-card,bitclock-master = <&dailink0_master>;
simple-audio-card,frame-master = <&dailink0_master>;
simple-audio-card,cpu {
sound-dai = <&i2s2>;
};
dailink0_master: simple-audio-card,codec {
sound-dai = <&hdmi>;
};
};
};
&i2c4{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c4_pins_mx>;
pinctrl-1 = <&i2c4_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2c4 */
clocks = <&scmi_clk CK_SCMI_I2C4>;
resets = <&scmi_reset RST_SCMI_I2C4>;
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <400000>;
/delete-property/ dmas;
/delete-property/ dma-names;
hdmi-transmitter@39{
compatible = "sil,sii9022";
reg = <0x39>;
iovcc-supply = <&v3v3_hdmi>;
cvcc12-supply = <&v1v2_hdmi>;
reset-gpios = <&gpioe 8 GPIO_ACTIVE_LOW>;
interrupts = <1 IRQ_TYPE_EDGE_FALLING>;
interrupt-parent = <&gpiog>;
#sound-dai-cells = <0>;
sil,i2s-data-lanes = <0>;
/*clocks = <&mclk>;
clock-names = "mclk";*/
status = "okay";
ports{
#address-cells = <1>;
#size-cells = <0>;
port@0{
reg = <0>;
sii9022_in:endpoint{
remote-endpoint = <<dc_ep0_out>;
};
};
port@1{
reg = <1>;
sii9022_out:endpoint{
remote-endpoint = <&hdmi_connector_in>;
};
};
port@3{
reg = <3>;
sii9022_tx_endpoint:endpoint{
remote-endpoint = <&i2s2_endpoint>;
};
};
};
};
};
&i2s2{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2s2_pins_mx>;
pinctrl-1 = <&i2s2_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2s2 */
clocks = <&rcc SPI2>, <&rcc SPI2_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "i2sclk", "x8k", "x11k";
i2s2_port:port{
i2s2_endpoint:endpoint{
remote-endpoint = <&sii9022_tx_endpoint>;
dai-format = "i2s";
mclk-fs = <256>;
};
};
/* USER CODE END i2s2 */
};
2024-10-29 1:41 PM
Hi!
I solved the problem. Now I can hear sound from my SII9022A PHY.
I did not use ASoC Graph Card, instead I used Simple Card inside Linux kernel.
I post the Linux Device Tree in case if some one in the future want to play some music through the SII9022A.
// SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
/*
* Copyright (C) 2024, STMicroelectronics - All Rights Reserved
* Author: STM32CubeMX code generation for STMicroelectronics.
*/
/* For more information on Device Tree configuration, please refer to
* https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
/dts-v1/;
#include <dt-bindings/pinctrl/stm32-pinfunc.h>
#include "stm32mp151.dtsi"
#include "stm32mp15xa.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15-m4-srm.dtsi"
/* USER CODE BEGIN includes */
#include "stm32mp15-scmi.dtsi"
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/mfd/st,stpmic1.h>
/* USER CODE END includes */
/ {
model = "STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26";
compatible = "st,stm32mp151a-stm32-computer-firmware-mx", "st,stm32mp151";
memory@c0000000 {
device_type = "memory";
reg = <0xc0000000 0x20000000>;
/* USER CODE BEGIN memory */
/* USER CODE END memory */
};
reserved-memory {
#address-cells = <1>;
#size-cells = <1>;
ranges;
/* USER CODE BEGIN reserved-memory */
optee@de000000 {
reg = <0xde000000 0x2000000>;
no-map;
};
mcuram2:mcuram2@10000000{
compatible = "shared-dma-pool";
reg = <0x10000000 0x40000>;
no-map;
};
vdev0vring0:vdev0vring0@10040000{
compatible = "shared-dma-pool";
reg = <0x10040000 0x1000>;
no-map;
};
vdev0vring1:vdev0vring1@10041000{
compatible = "shared-dma-pool";
reg = <0x10041000 0x1000>;
no-map;
};
vdev0buffer:vdev0buffer@10042000{
compatible = "shared-dma-pool";
reg = <0x10042000 0x4000>;
no-map;
};
mcu_rsc_table:mcu-rsc-table@10048000{
compatible = "shared-dma-pool";
reg = <0x10048000 0x8000>;
no-map;
};
mcuram:mcuram@30000000{
compatible = "shared-dma-pool";
reg = <0x30000000 0x40000>;
no-map;
};
retram:retram@38000000{
compatible = "shared-dma-pool";
reg = <0x38000000 0x10000>;
no-map;
};
/* USER CODE END reserved-memory */
};
/* USER CODE BEGIN root */
aliases{
ethernet0 = ðernet0;
serial0 = &uart4;
};
hdmi:connector{
compatible = "hdmi-connector";
#sound-dai-cells = <0>;
label = "hdmi";
type = "a";
port{
hdmi_connector_in:endpoint{
remote-endpoint = <&sii9022_out>;
};
hdmi_audio_out:endpoit{
remote-endpoint= <&sii9022_tx_endpoint>;
};
};
};
sound {
compatible = "simple-audio-card";
simple-audio-card,name = "SII9022A HDMI";
simple-audio-card,format = "i2s";
/*simple-audio-card,widgets = "Speaker", "External Speaker";
simple-audio-card,routing = "External Speaker", "LINE_OUT";*/
simple-audio-card,bitclock-master = <&dailink0_master>;
simple-audio-card,frame-master = <&dailink0_master>;
simple-audio-card,mclk-fs = <256>;
dailink0_master: simple-audio-card,cpu {
sound-dai = <&i2s2>;
};
simple-audio-card,codec {
sound-dai = <&sii9022A>;
};
};
config {
u-boot,boot-led = "heartbeat";
u-boot,error-led = "error";
u-boot,mmc-env-partition = "u-boot-env";
st,fastboot-gpios = <&gpioa 13 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
st,stm32prog-gpios = <&gpioa 14 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
};
led{
compatible = "gpio-leds";
led-blue{
label = "heartbeat";
gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;
linux,default-trigger = "timer"; /* Change from heartbeat -> timer */
default-state = "off";
};
led-red {
label = "error";
gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
default-state = "off";
};
};
vin:vin{
compatible = "regulator-fixed";
regulator-name = "vin";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
regulator-always-on;
};
chosen{
stdout-path = "serial0:115200n8";
};
/* USER CODE END root */
clocks{
/* USER CODE BEGIN clocks */
clk_csi: clk-csi {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <4000000>;
};
clk_hse: clk-hse {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <24000000>;
};
clk_hsi: clk-hsi {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <64000000>;
};
clk_lse: clk-lse {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <32768>;
};
clk_lsi: clk-lsi {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <32000>;
};
/* USER CODE END clocks */
};
}; /*root*/
&pinctrl {
eth1_pins_mx: eth1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_RX_CLK */
<STM32_PINMUX('A', 7, AF11)>, /* ETH1_RX_CTL */
<STM32_PINMUX('B', 0, AF11)>, /* ETH1_RXD2 */
<STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
<STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
<STM32_PINMUX('H', 7, AF11)>; /* ETH1_RXD3 */
bias-disable;
};
pins2 {
pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
pins3 {
pinmux = <STM32_PINMUX('B', 11, AF11)>, /* ETH1_TX_CTL */
<STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
<STM32_PINMUX('C', 2, AF11)>, /* ETH1_TXD2 */
<STM32_PINMUX('E', 2, AF11)>, /* ETH1_TXD3 */
<STM32_PINMUX('G', 4, AF11)>, /* ETH1_GTX_CLK */
<STM32_PINMUX('G', 5, AF11)>, /* ETH1_CLK125 */
<STM32_PINMUX('G', 13, AF11)>, /* ETH1_TXD0 */
<STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
bias-disable;
drive-push-pull;
slew-rate = <2>;
};
pins4 {
pinmux = <STM32_PINMUX('B', 5, AF0)>; /* ETH1_CLK */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
};
eth1_sleep_pins_mx: eth1_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_RX_CLK */
<STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
<STM32_PINMUX('A', 7, ANALOG)>, /* ETH1_RX_CTL */
<STM32_PINMUX('B', 0, ANALOG)>, /* ETH1_RXD2 */
<STM32_PINMUX('B', 5, ANALOG)>, /* ETH1_CLK */
<STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_TX_CTL */
<STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
<STM32_PINMUX('C', 2, ANALOG)>, /* ETH1_TXD2 */
<STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RXD0 */
<STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RXD1 */
<STM32_PINMUX('E', 2, ANALOG)>, /* ETH1_TXD3 */
<STM32_PINMUX('G', 4, ANALOG)>, /* ETH1_GTX_CLK */
<STM32_PINMUX('G', 5, ANALOG)>, /* ETH1_CLK125 */
<STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_TXD0 */
<STM32_PINMUX('G', 14, ANALOG)>, /* ETH1_TXD1 */
<STM32_PINMUX('H', 7, ANALOG)>; /* ETH1_RXD3 */
};
};
hdmi_cec_pins_mx: hdmi_cec_mx-0 {
pins {
pinmux = <STM32_PINMUX('B', 6, AF5)>; /* CEC */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
hdmi_cec_sleep_pins_mx: hdmi_cec_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('B', 6, ANALOG)>; /* CEC */
};
};
i2c1_pins_mx: i2c1_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 12, AF5)>, /* I2C1_SCL */
<STM32_PINMUX('D', 13, AF5)>; /* I2C1_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
i2c1_sleep_pins_mx: i2c1_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 12, ANALOG)>, /* I2C1_SCL */
<STM32_PINMUX('D', 13, ANALOG)>; /* I2C1_SDA */
};
};
i2c4_pins_mx: i2c4_mx-0 {
pins {
pinmux = <STM32_PINMUX('F', 14, AF4)>, /* I2C4_SCL */
<STM32_PINMUX('F', 15, AF4)>; /* I2C4_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
i2c4_sleep_pins_mx: i2c4_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('F', 14, ANALOG)>, /* I2C4_SCL */
<STM32_PINMUX('F', 15, ANALOG)>; /* I2C4_SDA */
};
};
i2s2_pins_mx: i2s2_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 9, AF5)>, /* I2S2_CK */
<STM32_PINMUX('B', 12, AF5)>, /* I2S2_WS */
<STM32_PINMUX('I', 3, AF5)>; /* I2S2_SDO */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
};
i2s2_sleep_pins_mx: i2s2_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 9, ANALOG)>, /* I2S2_CK */
<STM32_PINMUX('B', 12, ANALOG)>, /* I2S2_WS */
<STM32_PINMUX('I', 3, ANALOG)>; /* I2S2_SDO */
};
};
ltdc_pins_mx: ltdc_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 3, AF14)>, /* LTDC_B5 */
<STM32_PINMUX('B', 1, AF14)>, /* LTDC_G0 */
<STM32_PINMUX('B', 8, AF14)>, /* LTDC_B6 */
<STM32_PINMUX('C', 0, AF14)>, /* LTDC_R5 */
<STM32_PINMUX('D', 8, AF14)>, /* LTDC_B7 */
<STM32_PINMUX('D', 9, AF14)>, /* LTDC_B0 */
<STM32_PINMUX('D', 10, AF14)>, /* LTDC_B3 */
<STM32_PINMUX('E', 6, AF14)>, /* LTDC_G1 */
<STM32_PINMUX('E', 15, AF14)>, /* LTDC_R7 */
<STM32_PINMUX('F', 10, AF14)>, /* LTDC_DE */
<STM32_PINMUX('G', 10, AF14)>, /* LTDC_B2 */
<STM32_PINMUX('G', 12, AF14)>, /* LTDC_B1 */
<STM32_PINMUX('H', 2, AF14)>, /* LTDC_R0 */
<STM32_PINMUX('H', 3, AF14)>, /* LTDC_R1 */
<STM32_PINMUX('H', 8, AF14)>, /* LTDC_R2 */
<STM32_PINMUX('H', 9, AF14)>, /* LTDC_R3 */
<STM32_PINMUX('H', 10, AF14)>, /* LTDC_R4 */
<STM32_PINMUX('H', 12, AF14)>, /* LTDC_R6 */
<STM32_PINMUX('H', 13, AF14)>, /* LTDC_G2 */
<STM32_PINMUX('H', 14, AF14)>, /* LTDC_G3 */
<STM32_PINMUX('H', 15, AF14)>, /* LTDC_G4 */
<STM32_PINMUX('I', 0, AF14)>, /* LTDC_G5 */
<STM32_PINMUX('I', 1, AF14)>, /* LTDC_G6 */
<STM32_PINMUX('I', 2, AF14)>, /* LTDC_G7 */
<STM32_PINMUX('I', 4, AF14)>, /* LTDC_B4 */
<STM32_PINMUX('I', 9, AF14)>, /* LTDC_VSYNC */
<STM32_PINMUX('I', 10, AF14)>; /* LTDC_HSYNC */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
pins2 {
pinmux = <STM32_PINMUX('G', 7, AF14)>; /* LTDC_CLK */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
};
ltdc_sleep_pins_mx: ltdc_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 3, ANALOG)>, /* LTDC_B5 */
<STM32_PINMUX('B', 1, ANALOG)>, /* LTDC_G0 */
<STM32_PINMUX('B', 8, ANALOG)>, /* LTDC_B6 */
<STM32_PINMUX('C', 0, ANALOG)>, /* LTDC_R5 */
<STM32_PINMUX('D', 8, ANALOG)>, /* LTDC_B7 */
<STM32_PINMUX('D', 9, ANALOG)>, /* LTDC_B0 */
<STM32_PINMUX('D', 10, ANALOG)>, /* LTDC_B3 */
<STM32_PINMUX('E', 6, ANALOG)>, /* LTDC_G1 */
<STM32_PINMUX('E', 15, ANALOG)>, /* LTDC_R7 */
<STM32_PINMUX('F', 10, ANALOG)>, /* LTDC_DE */
<STM32_PINMUX('G', 7, ANALOG)>, /* LTDC_CLK */
<STM32_PINMUX('G', 10, ANALOG)>, /* LTDC_B2 */
<STM32_PINMUX('G', 12, ANALOG)>, /* LTDC_B1 */
<STM32_PINMUX('H', 2, ANALOG)>, /* LTDC_R0 */
<STM32_PINMUX('H', 3, ANALOG)>, /* LTDC_R1 */
<STM32_PINMUX('H', 8, ANALOG)>, /* LTDC_R2 */
<STM32_PINMUX('H', 9, ANALOG)>, /* LTDC_R3 */
<STM32_PINMUX('H', 10, ANALOG)>, /* LTDC_R4 */
<STM32_PINMUX('H', 12, ANALOG)>, /* LTDC_R6 */
<STM32_PINMUX('H', 13, ANALOG)>, /* LTDC_G2 */
<STM32_PINMUX('H', 14, ANALOG)>, /* LTDC_G3 */
<STM32_PINMUX('H', 15, ANALOG)>, /* LTDC_G4 */
<STM32_PINMUX('I', 0, ANALOG)>, /* LTDC_G5 */
<STM32_PINMUX('I', 1, ANALOG)>, /* LTDC_G6 */
<STM32_PINMUX('I', 2, ANALOG)>, /* LTDC_G7 */
<STM32_PINMUX('I', 4, ANALOG)>, /* LTDC_B4 */
<STM32_PINMUX('I', 9, ANALOG)>, /* LTDC_VSYNC */
<STM32_PINMUX('I', 10, ANALOG)>; /* LTDC_HSYNC */
};
};
sdmmc2_pins_mx: sdmmc2_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
<STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('E', 3, AF9)>, /* SDMMC2_CK */
<STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-pull-up;
drive-push-pull;
slew-rate = <1>;
};
};
sdmmc2_opendrain_pins_mx: sdmmc2_opendrain_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
<STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
bias-pull-up;
drive-push-pull;
slew-rate = <1>;
};
pins3 {
pinmux = <STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-pull-up;
drive-open-drain;
slew-rate = <1>;
};
};
sdmmc2_sleep_pins_mx: sdmmc2_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 8, ANALOG)>, /* SDMMC2_D4 */
<STM32_PINMUX('B', 3, ANALOG)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, ANALOG)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 9, ANALOG)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 14, ANALOG)>, /* SDMMC2_D0 */
<STM32_PINMUX('B', 15, ANALOG)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, ANALOG)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 3, ANALOG)>, /* SDMMC2_CK */
<STM32_PINMUX('E', 5, ANALOG)>, /* SDMMC2_D6 */
<STM32_PINMUX('G', 6, ANALOG)>; /* SDMMC2_CMD */
};
};
uart4_pins_mx: uart4_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
bias-pull-up;
};
pins2 {
pinmux = <STM32_PINMUX('G', 11, AF6)>; /* UART4_TX */
bias-pull-up;
drive-push-pull;
slew-rate = <0>;
};
};
uart4_idle_pins_mx: uart4_idle_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
bias-pull-up;
};
pins2 {
pinmux = <STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
bias-pull-up;
};
};
uart4_sleep_pins_mx: uart4_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('B', 2, ANALOG)>, /* UART4_RX */
<STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
bias-pull-up;
};
};
usb_otg_hs_pins_mx: usb_otg_hs_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
};
};
usb_otg_hs_sleep_pins_mx: usb_otg_hs_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
};
};
/* USER CODE BEGIN pinctrl */
/* USER CODE END pinctrl */
};
&pinctrl_z {
/* USER CODE BEGIN pinctrl_z */
/* USER CODE END pinctrl_z */
};
&m4_rproc{
status = "disabled";
/* USER CODE BEGIN m4_rproc */
resets = <&scmi_reset RST_SCMI_MCU>, <&scmi_reset RST_SCMI_MCU_HOLD_BOOT>;
reset-names = "mcu_rst", "hold_boot";
/*/delete-property/ st,syscfg-holdboot;*/
mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>, <&ipcc 3>;
mbox-names = "vq0", "vq1", "shutdown", "detach";
memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>, <&vdev0vring1>, <&vdev0buffer>, <&mcu_rsc_table>;
interrupt-parent = <&exti>;
interrupts = <68 1>;
wakeup-source;
/* USER CODE END m4_rproc */
m4_system_resources{
status = "disabled";
/* USER CODE BEGIN m4_system_resources */
/* USER CODE END m4_system_resources */
};
};
&bsec{
status = "okay";
/* USER CODE BEGIN bsec */
/* USER CODE END bsec */
};
&cec{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&hdmi_cec_pins_mx>;
pinctrl-1 = <&hdmi_cec_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN cec */
/* USER CODE END cec */
};
&dma1{
status = "okay";
/* USER CODE BEGIN dma1 */
resets = <&scmi_reset RST_SCMI_MDMA>;
/* USER CODE END dma1 */
};
&dma2{
status = "disabled";
/* USER CODE BEGIN dma2 */
/* USER CODE END dma2 */
};
&dmamux1{
status = "okay";
dma-masters = <&dma1>;
dma-channels = <8>;
/* USER CODE BEGIN dmamux1 */
/* USER CODE END dmamux1 */
};
ðernet0{
pinctrl-names = "default", "sleep";
pinctrl-0 = <ð1_pins_mx>;
pinctrl-1 = <ð1_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ethernet0 */
phy-mode = "rgmii-id";
max-speed = <1000>;
phy-handle = <&phy0>;
nvmem-cells = <ðernet_mac_address>;
nvmem-cell-names = "mac-address";
mdio{
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0:ethernet-phy@0{
reg = <0>;
};
};
/* USER CODE END ethernet0 */
};
&hsem{
status = "okay";
/* USER CODE BEGIN hsem */
/* USER CODE END hsem */
};
&i2c1{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c1_pins_mx>;
pinctrl-1 = <&i2c1_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2c1 */
/* USER CODE END i2c1 */
};
&i2c4{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c4_pins_mx>;
pinctrl-1 = <&i2c4_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2c4 */
clocks = <&scmi_clk CK_SCMI_I2C4>;
resets = <&scmi_reset RST_SCMI_I2C4>;
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <400000>;
/delete-property/ dmas;
/delete-property/ dma-names;
sii9022A: hdmi-transmitter@39{
compatible = "sil,sii9022";
reg = <0x39>;
iovcc-supply = <&v3v3_hdmi>;
cvcc12-supply = <&v1v2_hdmi>;
reset-gpios = <&gpioe 8 GPIO_ACTIVE_LOW>;
interrupts = <1 IRQ_TYPE_EDGE_FALLING>;
interrupt-parent = <&gpiog>;
#sound-dai-cells = <0>;
sil,i2s-data-lanes = <0>;
/*clocks = <&mclk>;
clock-names = "mclk";*/
status = "okay";
ports{
#address-cells = <1>;
#size-cells = <0>;
port@0{
reg = <0>;
sii9022_in:endpoint{
remote-endpoint = <<dc_ep0_out>;
};
};
port@1{
reg = <1>;
sii9022_out:endpoint{
remote-endpoint = <&hdmi_connector_in>;
};
};
port@3{
reg = <3>;
sii9022_tx_endpoint:endpoint{
remote-endpoint = <&i2s2_endpoint>;
};
};
};
};
pmic:stpmic@33{
compatible = "st,stpmic1";
reg = <0x33>;
/*interrupts-extended = <&gpioa 0 IRQ_TYPE_EDGE_FALLING>;*/
interrupts-extended = <&exti 55 IRQ_TYPE_EDGE_FALLING>;
interrupt-controller;
#interrupt-cells = <2>;
status = "okay";
regulators{
compatible = "st,stpmic1-regulators";
buck1-supply = <&vin>;
buck2-supply = <&vin>;
buck3-supply = <&vin>;
buck4-supply = <&vin>;
/*ldo1-supply = <&v3v3>;*/
ldo2-supply = <&vin>;
ldo3-supply = <&vdd_ddr>;
ldo4-supply = <&vin>;
ldo5-supply = <&vin>;
ldo6-supply = <&v3v3>;
vref_ddr-supply = <&vin>;
/*boost-supply = <&vin>;
pwr_sw1-supply = <&bst_out>;
pwr_sw2-supply = <&bst_out>;*/
vddcore:buck1{
regulator-name = "vddcore";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
vdd_ddr:buck2{
regulator-name = "vdd_ddr";
regulator-min-microvolt = <1350000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
vdd:buck3{
regulator-name = "vdd";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
st,mask-reset;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
v3v3:buck4{
regulator-name = "v3v3";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
regulator-over-current-protection;
regulator-initial-mode = <0>;
};
/*
v1v8_audio:ldo1{
regulator-name = "v1v8_audio";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
interrupts = <IT_CURLIM_LDO1 0>;
};*/
v3v3_hdmi:ldo2{
regulator-name = "v3v3_hdmi";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
interrupts = <IT_CURLIM_LDO2 0>;
};
vtt_ddr:ldo3{
regulator-name = "vtt_ddr";
regulator-min-microvolt = <500000>;
regulator-max-microvolt = <750000>;
regulator-always-on;
regulator-over-current-protection;
};
vdd_usb:ldo4{
regulator-name = "vdd_usb";
interrupts = <IT_CURLIM_LDO4 0>;
};
vdda:ldo5{
regulator-name = "vdda";
regulator-min-microvolt = <2900000>;
regulator-max-microvolt = <2900000>;
interrupts = <IT_CURLIM_LDO5 0>;
regulator-boot-on;
};
v1v2_hdmi:ldo6{
regulator-name = "v1v2_hdmi";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1200000>;
regulator-always-on;
interrupts = <IT_CURLIM_LDO6 0>;
};
vref_ddr:vref-ddr{
regulator-name = "vref_ddr";
regulator-always-on;
};
/*
bst_out:boost{
regulator-name = "bst_out";
interrupts = <IT_OCP_BOOST 0>;
};
vbus_otg:pwr-sw1{
regulator-name = "vbus_otg";
interrupts = <IT_OCP_OTG 0>;
};
vbus_sw:pwr-sw2{
regulator-name = "vbus_sw";
interrupts = <IT_OCP_SWOUT 0>;
regulator-active-discharge = <1>;
};
*/
};
onkey{
compatible = "st,stpmic1-onkey";
interrupts = <IT_PONKEY_F 0>, <IT_PONKEY_R 0>;
interrupt-names = "onkey-falling", "onkey-rising";
power-off-time-sec = <10>;
status = "okay";
};
};
/* USER CODE END i2c4 */
};
&i2s2{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2s2_pins_mx>;
pinctrl-1 = <&i2s2_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2s2 */
clocks = <&rcc SPI2>, <&rcc SPI2_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "i2sclk", "x8k", "x11k";
i2s2_port:port{
i2s2_endpoint:endpoint{
remote-endpoint = <&sii9022_tx_endpoint>;
dai-format = "i2s";
mclk-fs = <256>;
};
};
/* USER CODE END i2s2 */
};
<dc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_pins_mx>;
pinctrl-1 = <<dc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ltdc */
port{
ltdc_ep0_out:endpoint{
remote-endpoint = <&sii9022_in>;
};
};
/* USER CODE END ltdc */
};
&m4_dma2{
status = "okay";
/* USER CODE BEGIN m4_dma2 */
/* USER CODE END m4_dma2 */
};
&mdma1{
status = "okay";
/* USER CODE BEGIN mdma1 */
/* USER CODE END mdma1 */
};
&pwr_regulators{
status = "okay";
/* USER CODE BEGIN pwr_regulators */
vdd-supply = <&vdd>;
vdd_3v3_usbfs-supply = <&vdd_usb>;
/* USER CODE END pwr_regulators */
};
&rcc{
status = "okay";
/* USER CODE BEGIN rcc */
compatible = "st,stm32mp1-rcc-secure", "syscon";
clock-names = "hse", "hsi", "csi", "lse", "lsi";
clocks = <&scmi_clk CK_SCMI_HSE>,
<&scmi_clk CK_SCMI_HSI>,
<&scmi_clk CK_SCMI_CSI>,
<&scmi_clk CK_SCMI_LSE>,
<&scmi_clk CK_SCMI_LSI>;
/* USER CODE END rcc */
};
&rng1{
status = "okay";
/* USER CODE BEGIN rng1 */
clocks = <&scmi_clk CK_SCMI_RNG1>;
resets = <&scmi_reset RST_SCMI_RNG1>;
/* USER CODE END rng1 */
};
&rtc{
status = "okay";
/* USER CODE BEGIN rtc */
clocks = <&scmi_clk CK_SCMI_RTCAPB>, <&scmi_clk CK_SCMI_RTC>;
/* USER CODE END rtc */
};
&sdmmc2{
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc2_pins_mx>;
pinctrl-1 = <&sdmmc2_opendrain_pins_mx>;
pinctrl-2 = <&sdmmc2_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc2 */
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&v3v3>;
vqmmc-supply = <&vdd>;
mmc-ddr-3_3v;
/* USER CODE END sdmmc2 */
};
&tamp{
status = "okay";
/* USER CODE BEGIN tamp */
/* USER CODE END tamp */
};
&uart4{
pinctrl-names = "default", "idle", "sleep";
pinctrl-0 = <&uart4_pins_mx>;
pinctrl-1 = <&uart4_idle_pins_mx>;
pinctrl-2 = <&uart4_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN uart4 */
/delete-property/ dmas;
/delete-property/ dma-names;
u-boot,dm-pre-reloc;
/* USER CODE END uart4 */
};
&usbh_ehci{
status = "okay";
/* USER CODE BEGIN usbh_ehci */
phys = <&usbphyc_port0>;
#address-cells = <1>;
#size-cells = <0>;
/* onboard HUB */
hub@1 {
compatible = "usb424,2514";
reg = <1>;
vdd-supply = <&v3v3>;
};
/* USER CODE END usbh_ehci */
};
&usbh_ohci{
status = "okay";
/* USER CODE BEGIN usbh_ohci */
/* USER CODE END usbh_ohci */
};
&usbotg_hs{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&usb_otg_hs_pins_mx>;
pinctrl-1 = <&usb_otg_hs_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN usbotg_hs */
phys = <&usbphyc_port1 0>;
phy-names = "usb2-phy";
usb-role-switch;
u-boot,dm-pre-reloc;
u-boot,force-b-session-valid;
hnp-srp-disable;
dr_mode = "peripheral";
/* USER CODE END usbotg_hs */
};
&usbphyc{
status = "okay";
/* USER CODE BEGIN usbphyc */
phy-supply = <&vdd_usb>;
/* USER CODE END usbphyc */
};
&usbphyc_port0{
status = "okay";
/* USER CODE BEGIN usbphyc_port0 */
phy-supply = <&vdd_usb>;
st,tune-hs-dc-level = <2>;
st,enable-fs-rftime-tuning;
st,enable-hs-rftime-reduction;
st,trim-hs-current = <15>;
st,trim-hs-impedance = <1>;
st,tune-squelch-level = <3>;
st,tune-hs-rx-offset = <2>;
st,no-lsfs-sc;
/* USER CODE END usbphyc_port0 */
};
&usbphyc_port1{
status = "okay";
/* USER CODE BEGIN usbphyc_port1 */
phy-supply = <&vdd_usb>;
st,tune-hs-dc-level = <2>;
st,enable-fs-rftime-tuning;
st,enable-hs-rftime-reduction;
st,trim-hs-current = <15>;
st,trim-hs-impedance = <1>;
st,tune-squelch-level = <3>;
st,tune-hs-rx-offset = <2>;
st,no-lsfs-sc;
/* USER CODE END usbphyc_port1 */
};
/* USER CODE BEGIN addons */
/*
&arm_wdt{
timeout-sec = <32>;
status = "okay";
};
*/
&cpu0 {
cpu-supply = <&vddcore>;
clocks = <&scmi_clk CK_SCMI_MPU>;
};
&uart4_pins_mx {
u-boot,dm-pre-reloc;
pins1 {
u-boot,dm-pre-reloc;
};
pins2 {
u-boot,dm-pre-reloc;
};
};
&gpioz {
clocks = <&scmi_clk CK_SCMI_GPIOZ>;
};
/* USER CODE END addons */