2019-08-31 1:54 AM
I already tried the site of st wiki. I only want to get to run the starter package for my work at the university.
I saw that you can flash the sd-card wit windows-os.
Is that right?
I did it with CubeMxProgrammer. And the terminal said programming was succesfully.
After I changed the switches on the backside. The Display stays black.
Any ideas ?
Regards
Max
Solved! Go to Solution.
2019-09-02 8:41 AM
Hi @AndreyN
Your understanding of the DSI black screen issue 6 month back is not correct.
It was not a wrong connection to HDMI even if no cable but a timing issue during DSI screen initialization.
Anyway this is now fix in delivered software and should not happen any more.
Olivier
2019-09-01 11:34 PM
Hello,
I assume you are using DK2 board.
2019-09-02 12:55 AM
Hi Max,
Since you did not specify which board you are using, the following hint might be relevant for you or not.
I have similar problem with my stm32mp157c-dk2 board after flashing new image built with provided Yocto SDK. The attached display remains black. However, if you attach HDMI display, you might see the output there. As mentioned 6 months ago in other thread, there is a problem with current Yocto-based SDK resulting in output going to HDMI even if no cable attached.
Regards,
Andrey.
Edit: add link to HDMI problem discussion thread
2019-09-02 8:41 AM
Hi @AndreyN
Your understanding of the DSI black screen issue 6 month back is not correct.
It was not a wrong connection to HDMI even if no cable but a timing issue during DSI screen initialization.
Anyway this is now fix in delivered software and should not happen any more.
Olivier
2019-09-02 8:56 AM
Thanks for your comments Oliver.
> Anyway this is now fix in delivered software and should not happen any more.
Well, I built default weston image as well as eglfs/qt image using rather recent version of the provided Yocto SDK (download about two weeks ago). In both cases I still can not see output on DSI screen (hdmi works). However, the image on provided SD card works as expected. So I am confident that hardware is OK.
I will try to pull the latest version and see if it helps.
Thanks,
Andrey.
2019-09-02 9:00 AM
Hello PatrickF,
thank you for all of the ideas. Yes that is correct. I use the STM32MP157C-DK2.
And yes it was the ST-Link FW Version. I had an older one. Now it works!
Thank you very much!
Matix
2019-09-06 4:58 AM
For those who experience DSI display problems on stm32mp157c-dk2 board, this question (and answer) might be relevant.