2021-09-15 2:45 AM
Hi,
I tried to let "en.FLASH-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar_v3.0.0" work on the ODYSSEY STM32MP157C board.
Please advise when will produce error : "
Starting version 244.5+
[ 5.236977] blk_update_request: I/O error, dev mmcblk1, sector 173056 op 0x1:(WRITE) flags 0x20800 phys_seg 1 prio class 0
[ 5.246675] Buffer I/O error on dev mmcblk1p4, logical block 0, lost sync page write
[ 5.254488] EXT4-fs (mmcblk1p4): I/O error while writing superblock
[ 5.260725] EXT4-fs (mmcblk1p4): mount failed
[ 5.269862] VFS: could not find a valid V7 on mmcblk1p4.
" and how to solve it.
The attachment is the output log.
Thanks,
QiZhang
Solved! Go to Solution.
2021-11-08 4:47 PM
Hi QiZhang,
try to reconfigure the booting partition of rootfs by adding the same UUID appearing in the err-log file.
Kind regards
Ibrahim Abdelaty
2021-09-15 6:53 AM
Hi zqizh.1 (Community Member)
I see this SOM has 2 possible boot, SDcard and emmc. Do you have the same error on both boot image?
As it is a non ST board, I guess you can post your question directly on the forum dedicated to this board. https://forum.seeedstudio.com/
Regards,
Olivier
2021-11-08 4:47 PM
Hi QiZhang,
try to reconfigure the booting partition of rootfs by adding the same UUID appearing in the err-log file.
Kind regards
Ibrahim Abdelaty