2024-01-12 5:33 PM
Are you planning to add Bare Metal mode for STM32MP15x to CubeIde?
For the STM32MP13x series, it is present.
2024-01-14 11:37 PM
Hello @Roman Andronov ,
Thank you for your interest concerning this topic.
Today we do not plan to deliver a Cube FW Package on STM32MP15 for A7 cortex. As STM32MP15 already features a M4 cortex on which you can program in bare metal, ST made the choice to not do it on cortex A.
Kind regards,
Erwan.
2024-12-05 9:39 PM
Why? M4 cannot play with USB interface.Looking forward to add Bare Metal mode for STM32MP15x to CubeIde feature.
2024-12-08 6:47 PM
ST's partners, come on!
Wishing ST technology to be far ahead in the industry!
Let's change the world together and make it a better place!