cancel
Showing results for 
Search instead for 
Did you mean: 

Always USB boot after POR, instead of EMMC boot

robin_elecgator
Associate II

On my custom board I have the following issue, when my board powers up it goes into USB DFU mode instead of booting to EMMC, despite the BOOT pins. When I reset the board manually by taking nrst down, it boots correctly. I followed AN5031. I have discrete SMPS for 3.3/1.2 and 1.35V. I have 10k pull ups on the nrst line with 0.1µF cap. NRST and NRST_CORE are connected to each other with a 0R resistor. The reset of the EMMC is also on that line. The supplies rise in about 500µs to the nominal output voltage. HSE is a 24 MHz oscillator.

Any ideas?

1 REPLY 1
PatrickF
ST Employee

Hello,

this is a know bug, which will be solved in future silicon revision.

Meanwhile, as an indication, Toshiba THGBMNG5D1LBAIL, THGBMDG5D1LBAIL, and Kingston EMMC04G-M627-X03U operate correctly on the STM32MP157C-EV1 board.

See ES0438: STM32MP151x/3x/7x device limitations

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.