2024-06-03 5:47 AM
Hello everyone,
I am trying to debug a custom board with STM32MP151 with WM8988 connected with SAI2, the connection is just as STM32MP15x-DK with except that there is no I2S to HDMI. The device tree configuration is a mimic of STM32MP15xx-dkx.dtsi. After bootup, the soundcard was created, and I can run alsamixer.
The problem is whenever I try to play a sound, the driver complains about cannot get MCLK because the freq passed to wm8988_set_dai_sysclk() is zero. The log messages shown that the asoc try to configure the dai, but it passed the wrong MCLK freq to wm8988 dai. I don't know why? Is there something I am missing in the device tree?
Also, I tried to enable DEBUG in stm32_sai_sub.c and find that stm32_sai_mclk_enable() may not be called because I cannot find “Enable master clock” in dmesg.
I am using openstlinux eco system 4, the distro version is 4.0.11.
Here is the snipet of the device tree.
&i2c4{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c4_pins_z_mx>;
pinctrl-1 = <&i2c4_sleep_pins_z_mx>;
status = "okay";
/* USER CODE BEGIN i2c4 */
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <100000>;
wm8988: wm8988@1b {
compatible = "wlf,wm8988";
#sound-dai-cells = <0>;
reg = <0x1b>;
status = "okay";
DBVDD-supply = <&v3v3>;
DCVDD-supply = <&v3v3>;
AVDD-supply = <&vcc_audio>;
HPVDD-supply = <&vcc_audio>;
clocks = <&sai2a>;
clock-names = "MCLK";
ports {
#address-cells = <1>;
#size-cells = <0>;
wm8988_tx_endpoint: port@0 {
reg = <0>;
remote-endpoint = <&sai2a_endpoint>;
frame-master;// = <&wm8988_tx_endpoint>;
bitclock-master;// = <&wm8988_tx_endpoint>;
};
wm8988_rx_endpoint: port@1 {
reg = <1>;
remote-endpoint = <&sai2b_endpoint>;
frame-master;// = <&wm8988_rx_endpoint>;
bitclock-master;// = <&wm8988_rx_endpoint>;
};
};
};
/* USER CODE END i2c4 */
};
&sai2{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&sai2a_pins_mx>, <&sai2b_pins_mx>;
pinctrl-1 = <&sai2a_sleep_pins_mx>, <&sai2b_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN sai2 */
clocks = <&rcc SAI2>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "x8k", "x11k";
/* USER CODE END sai2 */
sai2a: audio-controller@4400b004{
status = "okay";
/* USER CODE BEGIN sai2a */
#clock-cells = <0>;
dma-names = "tx";
sai2a_port: port {
sai2a_endpoint: endpoint {
remote-endpoint = <&wm8988_tx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
};
/* USER CODE END sai2a */
};
sai2b: audio-controller@4400b024{
status = "okay";
/* USER CODE BEGIN sai2b */
dma-names = "rx";
st,sync = <&sai2a 2>;
clocks = <&rcc SAI2_K>, <&sai2a>;
clock-names = "sai_ck", "MCLK";
sai2b_port: port {
sai2b_endpoint: endpoint {
remote-endpoint = <&wm8988_rx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
};
/* USER CODE END sai2b */
};
};
/ {
sound: sound {
compatible = "audio-graph-card";
// label = "BM32MP15-Audio-Card";
label = "STM32MP15DK";
widgets =
"Headphone", "Headphone Jack",
"Microphone", "Microphone Jack",
"Speaker", "Speaker External";
routing =
"Speaker External", "LOUT2",
"Speaker External", "ROUT2",
"Headphone Jack", "ROUT1",
"Headphone Jack", "LOUT1",
"Playback", "MCLK",
"Capture", "MCLK";
dais = <&sai2a_port &sai2b_port>;
status = "okay";
};
};
Here is the dmesg logs related to sai, codec, and card. The last six lines were outputed after I try to play a sound by 'speaker-test -t sine‘.
[ 35.334229] platform 4400b004.audio-controller: Fixing up cyclic dependency with 1-001b
[ 35.397741] spi_stm32 4000b000.spi: driver initialized (master mode)
[ 35.453774] platform 4400b024.audio-controller: Fixing up cyclic dependency with 1-001b
[ 35.588275] wm8988 1-001b: wm8988_i2c_probe
[ 35.591486] wm8988: probe of 1-001b failed with error 517
[ 35.651872] wm8988 1-001b: wm8988_i2c_probe
[ 35.655040] wm8988: probe of 1-001b failed with error 517
[ 37.854538] using random self ethernet address
[ 37.905182] using random host ethernet address
[ 38.125237] usb0: HOST MAC 04:5e:be:d5:a7:58
[ 38.148229] usb0: MAC da:21:72:16:95:ef
[ 38.158513] dwc2 49000000.usb-otg: bound driver configfs-gadget
[ 38.871318] wm8988 1-001b: wm8988_i2c_probe
[ 38.874543] wm8988: probe of 1-001b failed with error 517
[ 38.883777] st,stm32-sai-sub 4400b004.audio-controller: Register master clock sai2a_mclk
[ 38.919012] st,stm32-sai-sub 4400b024.audio-controller: 4400b024.audio-controller synchronized with audio-controller@4400b004
[ 38.919087] st,stm32-sai-sub 4400b024.audio-controller: sai->sai_mclk = -1001602112
[ 38.947195] wm8988 1-001b: wm8988_i2c_probe
[ 38.983375] wm8988 1-001b: wm8988->mclk_handle = c44cc700
[ 39.051048] st,stm32-sai-sub 4400b004.audio-controller: Masks tx/rx:0x3/0x3, slots:2, width:32
[ 39.051530] st,stm32-sai-sub 4400b004.audio-controller: fmt 1001
[ 39.052755] st,stm32-sai-sub 4400b024.audio-controller: Masks tx/rx:0x3/0x3, slots:2, width:32
[ 39.063902] st,stm32-sai-sub 4400b024.audio-controller: fmt 1001
[ 39.063952] st,stm32-sai-sub 4400b024.audio-controller: Synchronized SAI configured as slave
[ 39.589379] RESIZE-HELPER START
[ 40.099033] RESIZE-HELPER: Using systemd-growfs
[ 40.156450] EXT4-fs (mmcblk0p10): resizing filesystem from 753664 to 753664 blocks
[ 40.222898] EXT4-fs (mmcblk0p8): resizing filesystem from 65536 to 65536 blocks
[ 40.282788] EXT4-fs (mmcblk0p9): resizing filesystem from 16384 to 16384 blocks
[ 40.342421] EXT4-fs (mmcblk0p11): resizing filesystem from 727516 to 727518 blocks
[ 40.358282] EXT4-fs (mmcblk0p11): resized filesystem to 727518
[ 40.410548] Filesystem Size Used Avail Use% Mounted on
devtmpfs 178M 0 178M 0% /dev
/dev/mmcblk0p10 685M 125M 525M 20% /
tmpfs 245M 0 245M 0% /dev/shm
tmpfs 98M 8.6M 90M 9% /run
tmpfs 4.0M 0 4.0M 0% /sys/fs/cgroup
tmpfs 245M 0 245M 0% /tmp
/dev/mmcblk0p8 55M 13M 39M 25% /boot
/dev/mmcblk0p9 14M 6.0M 6.7M 48% /vendor
/dev/mmcblk0p11 660M 148K 620M 1% /usr/local
tmpfs 245M 0 245M 0% /var/volatile
[ 40.488909] RESIZE-HELPER FINISH
[ 40.906720] RESIZE-HELPER START
[ 41.013085] RESIZE-HELPER: Using systemd-growfs
[ 41.058996] EXT4-fs (mmcblk0p10): resizing filesystem from 753664 to 753664 blocks
[ 41.090163] EXT4-fs (mmcblk0p8): resizing filesystem from 65536 to 65536 blocks
[ 41.121164] EXT4-fs (mmcblk0p9): resizing filesystem from 16384 to 16384 blocks
[ 41.152169] EXT4-fs (mmcblk0p11): resizing filesystem from 727518 to 727518 blocks
[ 41.173337] Filesystem Size Used Avail Use% Mounted on
devtmpfs 178M 0 178M 0% /dev
/dev/mmcblk0p10 685M 125M 525M 20% /
tmpfs 245M 0 245M 0% /dev/shm
tmpfs 98M 8.6M 90M 9% /run
tmpfs 4.0M 0 4.0M 0% /sys/fs/cgroup
tmpfs 245M 0 245M 0% /tmp
/dev/mmcblk0p8 55M 13M 39M 25% /boot
/dev/mmcblk0p9 14M 6.0M 6.7M 48% /vendor
/dev/mmcblk0p11 660M 148K 620M 1% /usr/local
tmpfs 245M 0 245M 0% /var/volatile
[ 41.234053] RESIZE-HELPER FINISH
[ 44.718102] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 44.768910] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 45.237727] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:01] driver [RTL8211F Gigabit Ethernet] (irq=POLL)
[ 45.258267] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 45.275609] dwmac4: Master AXI performs any burst length
[ 45.287727] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 45.293887] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 45.334072] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 45.350189] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 48.570866] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 48.587664] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 280.586461] wm8988 1-001b: No MCLK configured, call set_sysclk() on init
[ 280.591971] wm8988 1-001b: ASoC: error at snd_soc_dai_startup on wm8988-hifi: -22
[ 280.605747] wm8988 1-001b: set sysclk, freq = 0
[ 280.612190] wm8988 1-001b: could not set sysclk, freq = 0
[ 280.616181] wm8988 1-001b: ASoC: error at snd_soc_dai_set_sysclk on wm8988-hifi: -22
[ 280.627751] 4400b004.audio-controller-wm8988-hifi: __soc_pcm_open() failed (-22)
Here is the lsmod output:
Module Size Used by
cfg80211 651264 0
stm32_adc 36864 0
stm32_timer_trigger 20480 1 stm32_adc
stm32_lptimer_trigger 16384 1 stm32_adc
snd_soc_stm32_sai_sub 28672 8
pwm_stm32 20480 0
snd_soc_audio_graph_card 16384 0
snd_soc_simple_card_utils 20480 1 snd_soc_audio_graph_card
stm32_adc_core 20480 0
stm32_timers 16384 1 pwm_stm32
snd_soc_stm32_sai 16384 0
spi_stm32 24576 0
usb_f_ncm 24576 2
u_ether 20480 1 usb_f_ncm
libcomposite 49152 10 usb_f_ncm
sch_fq_codel 20480 3
snd_soc_wm8988 28672 1
snd_soc_core 180224 4 snd_soc_audio_graph_card,snd_soc_wm8988,snd_soc_simple_card_utils,snd_soc_stm32_sai_sub
snd_pcm_dmaengine 16384 1 snd_soc_core
snd_pcm 94208 4 snd_pcm_dmaengine,snd_soc_wm8988,snd_soc_core,snd_soc_stm32_sai_sub
snd_timer 28672 1 snd_pcm
snd 53248 4 snd_timer,snd_soc_core,snd_pcm,snd_soc_stm32_sai_sub
soundcore 16384 1 snd
fusb302 28672 0
tcpm 65536 1 fusb302
typec 36864 1 tcpm
ip_tables 24576 0
x_tables 24576 1 ip_tables
ipv6 507904 28
Here is the output of clk_summary:
pll3 1 1 0 417755859 0 0 50000 Y
pll3_r 0 0 0 11290699 0 0 50000 N
pll3_q 0 0 0 24573875 0 0 47058 N
sai2_k 0 0 0 24573875 0 0 50000 N
sai2a_mclk 0 0 0 0 0 0 50000 ?
Here is the output of 'ls /dev/snd'
by-path controlC0 pcmC0D0p pcmC0D1c timer
Thanks and any comments would be appreciated.
Solved! Go to Solution.
2024-06-06 2:16 AM
Hi @jasonj2,
The sound / SAI / Codec DT configuration looks good.
Could you please cross-check the SAI2_MCLK PIN configuration (should be in sai2a_pins_mx) is aligned with your hardware ?
Do you have an idea about why it takes so much time for the codec to be probed ? I noticed a lot of PROBE_DEFER which means that the driver is waiting something.....
Regarding the MCLK error : I would check with a scope if the the MCLK is really there or not : it would help to understand if the problem comes from SAI (clock, pin muxing configuration), or from the codec.
BTW, did you check if function wm8988_set_dai_sysclk() was called during codec driver init ?
BR,
Christophe
2024-06-06 2:16 AM
Hi @jasonj2,
The sound / SAI / Codec DT configuration looks good.
Could you please cross-check the SAI2_MCLK PIN configuration (should be in sai2a_pins_mx) is aligned with your hardware ?
Do you have an idea about why it takes so much time for the codec to be probed ? I noticed a lot of PROBE_DEFER which means that the driver is waiting something.....
Regarding the MCLK error : I would check with a scope if the the MCLK is really there or not : it would help to understand if the problem comes from SAI (clock, pin muxing configuration), or from the codec.
BTW, did you check if function wm8988_set_dai_sysclk() was called during codec driver init ?
BR,
Christophe
2024-06-28 9:46 AM
(1) I checked the PIN configuration, I think it is right. Here is the PIN configuration for sai2a/b
sai2a_pins_mx: sai2a_mx-0 {
pins {
pinmux = <STM32_PINMUX('I', 4, AF10)>, /* SAI2_MCLK_A */
<STM32_PINMUX('I', 5, AF10)>, /* SAI2_SCK_A */
<STM32_PINMUX('I', 6, AF10)>, /* SAI2_SD_A */
<STM32_PINMUX('I', 7, AF10)>; /* SAI2_FS_A */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
};
sai2a_sleep_pins_mx: sai2a_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('I', 4, ANALOG)>, /* SAI2_MCLK_A */
<STM32_PINMUX('I', 5, ANALOG)>, /* SAI2_SCK_A */
<STM32_PINMUX('I', 6, ANALOG)>, /* SAI2_SD_A */
<STM32_PINMUX('I', 7, ANALOG)>; /* SAI2_FS_A */
};
};
sai2b_pins_mx: sai2b_mx-0 {
pins {
pinmux = <STM32_PINMUX('G', 10, AF10)>; /* SAI2_SD_B */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
};
sai2b_sleep_pins_mx: sai2b_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('G', 10, ANALOG)>; /* SAI2_SD_B */
};
};
(2) Yes, there is some PROBE_DEFER. I checked it, they are produced by wm8988_i2c_probe() because it cannot get MCLK from SAI (), but it looks it can finally get MCLK after tries. I don't know why.
wm8988->mclk_handle = devm_clk_get(&i2c->dev, "MCLK");
if (IS_ERR(wm8988->mclk_handle)) {
dev_err(&i2c->dev, "Failed to get MCLK from %s\n", dev_name(&i2c->dev));
if (PTR_ERR(wm8988->mclk_handle) != -ENOENT)
return PTR_ERR(wm8988->mclk_handle);
wm8988->mclk_handle = NULL;
}
(3) I confirm wm8988_set_dai_sysclk() was called with freq=0, because there are log looks like "wm8988 1-001b: could not set sysclk, freq = 0" which is a debug output I made in the source code.
Sorry, I clicked the "Accept as Solution" by mistake. The problem still remains.
Best regards,
JasonJ
2024-07-01 7:57 AM
Hello @jasonj2,
I will try to summarize :
- The SAI configuration looks good
- The Codec configuration looks good
- Several probe_defer because SAI doesn't seem to provide MCLK, but after a while, it seems to be there.
For me, we need to know if the MCLK signal is really there on the wire:
- if yes, we need to focus on the codec
- if no, we need to focus on SAI
- if no, and after a while yes, understand what is the event which enables the clock so late.
BR
Christophe