cancel
Showing results for 
Search instead for 
Did you mean: 

Using QT Ecosystem 2.0 - make-mod-script failed.

FBoar.1
Associate II

Hi All,

Please , I`m pretty new here but so far using standard layer it works correctly hover when trying to use the QT / Distro openstlinux-eglfs layers meta-st I`m getting error related to make-mod-scripts.

ERROR: Task (/local/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/layers/openembedded-core/meta/recipes-kernel/make-mod-scripts/make-mod-scripts_1.0.bb:do_configure) failed with exit code '1'

Can any good soul help-me on that ? Anything I can do here ?

Thank You so Much !

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @FBoar.1​ ,

More complete error traces maybe helpful to point the issue.

First hint is to double check you have properly installed all PC_Prerequisite.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.