2024-08-18 03:25 PM - edited 2024-08-18 03:38 PM
I have compiled.
And it seems to work well. I have also tried to implement a pre-made OpenSTLinux from the Source files. And it seems to work well too. I haven't got any terminal up and running. I can only see the display output of messages when I start it up.
Notice that the kernel comes from STM32MP157 and before the kernel startup, it's from STM32MP151. That's why you see that the MAC address is not set, but once linux kernel is started, you can see inside the log that the MAC address is set to "56:bf:8f:58:f8:31".
I need to create bootfs, vendorfs, userfs and rootfs.ext4, so what should I do next? Should I create empty .ext4 files and then mount the .ext4 files and later fill them with...?