2024-06-13 08:34 AM - last edited on 2024-06-13 11:41 PM by Peter BENSCH
HI There,
I am getting error installing wireguard in STM32mp135s. I have added wireguard-tool by adding in local.conf, its successfully builts. but when I add wireguard-module I get compilation error. So I skipped it wireguard-module. Some kernel setting also done for Wireguard by following this site https://www.wireguard.com/compilation/#kernel-requirements. When I try create inteface I get following error. What is the solution for this, how can I add wireguard in my build?
Error-
wg-quick up wg0
[#] ip link add wg0 type wireguard
[ 129.799785] wireguard: Unknown symbol curve25519_null_point (err -2)
[ 129.799834] wireguard: Unknown symbol udp_sock_create4 (err -2)
[ 129.799858] wireguard: Unknown symbol udp_tunnel6_xmit_skb (err -2)
Error: Unknown device type.
[ 129.799894] wireguard: Unknown symbol chacha20poly1305_encrypt_sg_inplace (er r -2)
[ 129.799939] wireguard: Unknown symbol chacha20poly1305_encrypt (err -2)
[ 129.800041] wireguard: Unknown symbol chacha20poly1305_decrypt_sg_inplace (er r -2)
[ 129.800076] wireguard: Unknown symbol xchacha20poly1305_encrypt (err -2)
[ 129.800084] wireguard: Unknown symbol xchacha20poly1305_decrypt (err -2)
[ 129.800105] wireguard: Unknown symbol udp_tunnel_sock_release (err -2)
Unable to access interface: Protocol not supported
[#] ip [ 129.800131] wireguard: Unknown symbol setup_udp_tunnel_sock (err -2)
link delete dev wg0
[ 129.800140] wireguard: Unknown symbol udp_sock_create6 (err -2)
[ 129.800171] wireguard: Unknown symbol curve25519_arch (err -2)
[ 129.800195] wireguard: Unknown symbol chacha20poly1305_decrypt (err -2)
[ 129.800220] wireguard: Unknown symbol curve25519_base_arch (err -2)
[ 129.800236] wireguard: Unknown symbol udp_tunnel_xmit_skb (err -2)
[ 129.871716] wireguard: Unknown symbol curve25519_null_point (err -2)
[ 129.871764] wireguard: Unknown symbol udp_sock_create4 (err -2)
Cannot find device "wg0"
root@stm32[ 129.871789] wireguard: Unknown symbol udp_tunnel6_xmit_skb (err -2)
[ 129.871826] wireguard: Unknown symbol chacha20poly1305_encrypt_sg_inplace (er r -2)
[ 129.871871] wireguard: Unknown symbol chacha20poly1305_encrypt (err -2)
[ 129.871972] wireguard: Unknown symbol chacha20poly1305_decrypt_sg_inplace (er r -2)
[ 129.872006] wireguard: Unknown symbol xchacha20poly1305_encrypt (err -2)
[ 129.872014] wireguard: Unknown symbol xchacha20poly1305_decrypt (err -2)
[ 129.872035] wireguard: Unknown symbol udp_tunnel_sock_release (err -2)
[ 129.872060] wireguard: Unknown symbol setup_udp_tunnel_sock (err -2)
[ 129.872069] wireguard: Unknown symbol udp_sock_create6 (err -2)
[ 129.872101] wireguard: Unknown symbol curve25519_arch (err -2)
[ 129.872126] wireguard: Unknown symbol chacha20poly1305_decrypt (err -2)
[ 129.872150] wireguard: Unknown symbol curve25519_base_arch (err -2)
[ 129.872167] wireguard: Unknown symbol udp_tunnel_xmit_skb (err -2)
mp13-rt:/etc/wireguard# modinfo chacha20poly1305
modinfo: ERROR: Module chacha20poly1305 not found.
root@stm32mp13-rt:/etc/wireguard#
2024-06-22 05:26 AM
Hello,
If anyone have specific solution for that? Kindly provide any solution for the same ASAP.