cancel
Showing results for 
Search instead for 
Did you mean: 

Communication between STM32MP1 A7 and STM32 over SPI

PVaaz.1
Associate III

Hello ,

Can anyone please point me to the example of SPI communication between stm32(F4/L0/L4) with A7 of STM32MP1?

A7 could be a driver or any user application but both should be able to send and receive the data over spi.

on A7 I suppose it will be SPI5.

please assist.

Thanks in advance!

Br,,

P

1 REPLY 1
PatrickF
ST Employee

Hi @PVaaz.1​ 

is those pages help you for a start point ?

https://wiki.st.com/stm32mpu/wiki/SPI_overview#API_description

https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev

Regards

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.