2024-08-26 3:34 PM
I tried to replace the uImage and .dtb file inside the starter package.
First I copied over the kernel and .dtb file.
sudo mount -o loop st-image-bootfs-openstlinux-weston-stm32mp1.ext4 /mnt/bootfs
sudo cp ../linux-6.1.82/build/arch/arm/boot/uImage /mnt/bootfs/
sudo cp ../linux-6.1.82/build/arch/arm/boot/dts/stm32mp151a-stm32-computer-firmware-mx.dtb /mnt/bootfs
sudo umount /mnt/bootfs
Then I booted the Linux kernel. See the log file log.txt. It stopped at the USB Hub decleration. So I guess that linux kernel was booted, but not initrd.
I tried to boot the system manually via U-boot and this happen.
STM32MP> part list mmc 0
Partition Map for MMC device 0 -- Partition Type: EFI
Part Start LBA End LBA Name
Attributes
Type GUID
Partition GUID
1 0x00000400 0x000007ff "metadata1"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: 92f0b426-e174-4bac-9287-019e4f858971
2 0x00000800 0x00000bff "metadata2"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: 31227fc6-8d76-4b65-a8be-90720614ecce
3 0x00000c00 0x00002bff "fip-a"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 4fd84c93-54ef-463f-a7ef-ae25ff887087
4 0x00002c00 0x00004bff "fip-b"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 09c54952-d5bf-45af-acee-335303766fb3
5 0x00004c00 0x00004fff "u-boot-env"
attrs: 0x0000000000000000
type: 3de21764-95bd-54bd-a5c3-4abe786f38a8
(u-boot-env)
guid: 2c809cbe-60fb-4bfd-abfb-20d86de1f22e
6 0x00005000 0x00024fff "bootfs"
attrs: 0x0000000000000004
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: b168bf89-4526-46f1-a200-9d9c2682a2ad
7 0x00025000 0x0002cfff "vendorfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: a7b0fddd-33cf-4516-a2ec-5c4bc237d80e
8 0x0002d000 0x0019cfff "rootfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: e91c4e10-16e6-4c0e-bd0e-77becf4a3582
9 0x0019d000 0x00e8fbff "userfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: 7bc0d1fe-94a1-461d-8ee4-bcefdcb68617
STM32MP> ext4ls mmc 0:6 /
<DIR> 2048 .
<DIR> 2048 ..
<DIR> 12288 lost+found
4187 boot.scr.uimg
<DIR> 1024 mmc0_extlinux
<DIR> 1024 mmc1_extlinux
<DIR> 1024 nand0_extlinux
7802 splash_landscape.bmp
89462 splash_portrait.bmp
6232362 st-image-resize-initrd
65603 stm32mp135f-dk-a7-examples.dtb
63622 stm32mp135f-dk.dtb
127101 stm32mp157a-dk1.dtb
135636 stm32mp157a-ev1.dtb
130031 stm32mp157c-dk2-a7-examples.dtb
130417 stm32mp157c-dk2-m4-examples.dtb
129643 stm32mp157c-dk2.dtb
122602 stm32mp157c-ed1.dtb
136313 stm32mp157c-ev1-a7-examples.dtb
136657 stm32mp157c-ev1-m4-examples.dtb
136078 stm32mp157c-ev1.dtb
127367 stm32mp157d-dk1-a7-examples.dtb
128105 stm32mp157d-dk1-m4-examples.dtb
127331 stm32mp157d-dk1.dtb
135909 stm32mp157d-ev1.dtb
130325 stm32mp157f-dk2-a7-examples.dtb
130711 stm32mp157f-dk2-m4-examples.dtb
129937 stm32mp157f-dk2.dtb
122832 stm32mp157f-ed1.dtb
136543 stm32mp157f-ev1-a7-examples.dtb
136887 stm32mp157f-ev1-m4-examples.dtb
136308 stm32mp157f-ev1.dtb
8249920 uImage
79018 stm32mp151a-stm32-computer-firmware-mx.dtb
STM32MP> ext4ls mmc 0:7 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
<DIR> 1024 lib
STM32MP> ext4ls mmc 0:8 /
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 16384 lost+found
<DIR> 4096 bin
<DIR> 4096 boot
<DIR> 4096 dev
<DIR> 4096 etc
<DIR> 4096 home
<DIR> 4096 lib
<DIR> 4096 media
<DIR> 4096 mnt
<DIR> 4096 proc
<DIR> 4096 run
<DIR> 4096 sbin
<DIR> 4096 srv
<DIR> 4096 sys
<DIR> 4096 tmp
<DIR> 4096 usr
<DIR> 4096 var
<DIR> 4096 vendor
STM32MP> ext4ls mmc 0:9 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
<DIR> 1024 Cube-M4-examples
<DIR> 1024 Linux-A7-examples
<DIR> 1024 demo
<DIR> 1024 weston-start-at-startup
STM32MP> ext4load mmc 0:6 0xC2000000 /uImage
8249920 bytes read in 955 ms (8.2 MiB/s)
STM32MP> ext4load mmc 0:6 0xC4000000 /stm32mp151a-stm32-computer-firmware-mx.dtb
79018 bytes read in 78 ms (989.3 KiB/s)
STM32MP> ext4load mmc 0:6 0xC6000000 /st-image-resize-initrd
6232362 bytes read in 738 ms (8.1 MiB/s)
STM32MP> bootm 0xC2000000 0xC6000000 0xC4000000
## Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-6.1.82
Created: 2024-08-26 20:05:23 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 8249856 Bytes = 7.9 MiB
Load Address: c2000040
Entry Point: c2000040
Verifying Checksum ... OK
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid
STM32MP>
I also did use another address for the Ramdisk file. Same result.
STM32MP> ext4load mmc 0:6 0xC8000000 /st-image-resize-initrd
6232362 bytes read in 739 ms (8 MiB/s)
STM32MP> bootm 0xC2000000 0xC8000000 0xC4000000
## Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-6.1.82
Created: 2024-08-26 20:05:23 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 8249856 Bytes = 7.9 MiB
Load Address: c2000040
Entry Point: c2000040
Verifying Checksum ... OK
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid
STM32MP>
So that means that the Ramdisk file is corrupted. Notice that I have another hardware, the MP151 series, instead of the MP157 series. Perhaps I need to build my own initrd?
Yes. I have replace the "old" ramdisk file with a new ram disk file, and I still get the same error.
Question:
Is there any way for me to manually boot a correct image of initrd file by building my own?