Skip to main content
MToum.1
Associate II
Aug 26, 2024 3:52 AM UTC
Solved

STM32MP1 and Codec Running as Slave with si5351B as Master clock on SAI

Hello,

I am wondering what could be the best way to write a device tree that sets the STM32MP1 as SAI SLAVE with a CODEC also running as SAI slave. The HW design I am studying has the following specs:

1) STM32MP1 with ALSA and one SAI interface.

2) A codec chipset running as SAI slave.

3) The Si5351B part running as a MASTER clock providing the SAI bit and frame (L/R) clocks to both the SoC and CODEC.

I understand such a setup is a little out of the norm. How can the device tree be modified on the SAI side to avoid the STM32MP1 to become a MASTER. The snippet of a possible device tree is below.

How can  I force the STM32MP1 to be a SLAVE on SAI?

I would imagine writing the device tree as follows:

 

&sai1{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&sai1b_pins_mx>;
pinctrl-1 = <&sai1b_sleep_pins_mx>;
status = "okay";

/* USER CODE BEGIN sai1 */
/* Specify external clock sources for SAI1
We MUST add the clock-names according to the doc. */
clocks = <&rcc SAI1>, <&rcc PLL3_Q>, <&rcc PLL3_R>, <&si5351b_clk0>, <&si5351b_clk1>;
clock-names = "pclk", "x8k", "x11k", "sclk", "lrclk";
/* USER CODE END sai1 */


sai1b:audio-controller@4400a024{
status = "okay";
/* USER CODE BEGIN sai1b */
dma-names = "tx";
mode = "i2s-slave"; /* Set SAI interface to slave mode */
sai1b_port: port {
sai1b_endpoint: endpoint {
remote-endpoint = <&CODEC_tx_endpoint>;
format = "i2s";
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
bitclock-master = <0>; /* SAI is not the bit clock master */
frame-master = <0>; /* SAI is not the frame sync master */
/* Synchronization configuration */
st,sync = "lrclk"; /* Synchronization signal source */

};
};
/* USER CODE END sai1b */
};
};

The couple of tests performed on a target device are showing that a similar device tree as above still put the STM32MP1 as a MASTER. 

Please comment on this.

I am also reading the driver code and the notion of EXTERNAL is unclear to me, are we talking about a signal External to SAI or External to the SoC?

 

The code reference for the ST driver is: https://github.com/STMicroelectronics/linux/blob/v5.15-stm32mp/sound/soc/stm/stm32_sai.c and https://github.com/STMicroelectronics/linux/blob/v5.15-stm32mp/sound/soc/stm/stm32_sai_sub.c

 

 

 

 

 

 

 

 

This topic has been closed for replies.
Christophe Guibout
ST Technical Moderator
Aug 28, 2024 8:35 AM UTC

Hello @MToum.1,

 

You need to remove these two lines from SAI DT entry to configure it as slave:

frame-master;

bitclock-master; 

 

Feel free to look into the SAI DT configuration wiki page.

The following page could help as well : Soundcard configuration.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Christophe Guibout
ST Technical Moderator
Aug 28, 2024 8:35 AM UTC

Hello @MToum.1,

 

You need to remove these two lines from SAI DT entry to configure it as slave:

frame-master;

bitclock-master; 

 

Feel free to look into the SAI DT configuration wiki page.

The following page could help as well : Soundcard configuration.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.