2021-04-16 7:01 AM
1) Where can I get information on these GPIOs ?
2) Can I safely reassign, say GPIOz ?
https://github.com/MYiR-Dev/myir-st-linux/blob/develop/arch/arm/boot/dts/stm32mp15xxac-pinctrl.dtsi
2021-04-28 8:33 AM
Hi,
all the GPIOs 'okay' you see are for the GPIO banks IP, which are enabled by default and handled by Linux side.
Changes in this file is not recommended.
Individual pin assignments within GPIO banks are define in other part of the device tree (e.g. output from CubeMx/CubeIDE like stm32mp157c-mydevicetree-mx.dts).
Please look at https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
Regards.