2024-07-20 6:46 PM
Hello,
I enabled the generation of debug filesystem by adding two variables in file build-openstlinuxweston-stm32mp15-disco/conf/local.conf as shown below to use with GDB. This step is also mentioned in Yocto documentation (Link: https://docs.yoctoproject.org/dev/dev-manual/debugging.html#using-the-gdbserver-method ).
IMAGE_GEN_DEBUGFS = "1"
IMAGE_FSTYPES_DEBUGFS = "tar.bz2"
When this option is enabled I get below dependency(?) error,
Does anyone know how to fix this?
Additional information:
Target HW : STM32MP157F-DK2
Target image : st-image-weston
Thanks,
Solved! Go to Solution.
2024-07-26 9:27 PM
After few research I got to know that the problem comes from the PACKAGE_CLASSES. Changing the default PACKAGE_CLASSES in local.conf from package_deb to package_ipk fixed the issue.
# force the usage of debian package
#PACKAGE_CLASSES = "package_deb"
PACKAGE_CLASSES = "package_ipk"
2024-07-22 1:08 AM
Hi @gmax,
If you want to use GDB, I could suggest that you have a look at the STM32 MPU wiki (https://wiki.st.com/stm32mpu/wiki/Main_Page).
The following articles might be interesting for you:
I’m aware that the above information doesn’t fix the problem that you highlighted, but nevertheless, I hope it might help.
Regards,
JC.
2024-07-23 4:52 AM
Hello @Jean-Christophe_TROTIN ,
Thanks for your reply. I did read those articles before but it mostly speak about how to use GDB rather than how to build for debug. Looks like I may need to switch from Distribution package to Developer package.
Thanks,
gmax
2024-07-26 9:27 PM
After few research I got to know that the problem comes from the PACKAGE_CLASSES. Changing the default PACKAGE_CLASSES in local.conf from package_deb to package_ipk fixed the issue.
# force the usage of debian package
#PACKAGE_CLASSES = "package_deb"
PACKAGE_CLASSES = "package_ipk"