2024-06-12 03:58 AM - edited 2024-06-12 04:42 AM
Hi,all
I noticed that the ethernet driver stm32mp13xx_hal_eth.c in the STM32CubeMP13_V1.1.0 already supports PTP,
When will STM32CubeMP2 package be available, and since the STM32MP2 series supports TSN, whether EST(IEEE 802.1Qbv) and FPE(IEEE802.1Qbu) functions are supported in the driver?
@MWB_CHa ,I see that PTP function is added by you, so do you know the relevant information?
Solved! Go to Solution.
2024-06-14 05:56 AM
Hi @CosmicRoach
there is no plan to provide an STM32CubeMP2 bare-metal package for STM32MP25 (only Linux and Android).
Maybe foreseen for future lower cost/perf derivatives such as STM32MP21, but development is not yet confirmed.
Regards.
2024-06-14 05:56 AM
Hi @CosmicRoach
there is no plan to provide an STM32CubeMP2 bare-metal package for STM32MP25 (only Linux and Android).
Maybe foreseen for future lower cost/perf derivatives such as STM32MP21, but development is not yet confirmed.
Regards.
2024-06-16 06:41 PM
Thanks for the reply, I'll stay tuned.