cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP257F-EV1 STLinux Packages: Serial command line

mfny
Associate II

Hello,

I am wondering can the ST Linux Starter Package(or indeed any of the STLinux packages) be interacted with via a command line via serial port and if so how would this be set up ? as the additional display for this board is unavailable to me.

1 REPLY 1
PatrickF
ST Employee

Hi @mfny 

for sure, the Starter Package console is available thru STLINK. This is the main control interface to Linux (for tests or install additional packages).

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Let%27s_start/Unpack_the_STM32MP257x-EV1_board#Board_connections

Just connect USB Type-C CN21 to a PC and you will have 2 x VCP available (one for Cortex-A35 Console, the second optional for Cortex-M33 console).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.