cancel
Showing results for 
Search instead for 
Did you mean: 

"panel-simple.c" customization errors

nataut
Associate III

This post is connected to my previous one "Display customization". I created this new post because I can't insert replies in the previous one "Display customization"

I created the following patch to modify the panel-simple.c file 

diff --git a/drivers/gpu/drm/panel/panel-simple.c b/drivers/gpu/drm/panel/panel-simple.c index 654fea2..8e4234f 100644 --- a/drivers/gpu/drm/panel/panel-simple.c +++ b/drivers/gpu/drm/panel/panel-simple.c @@ -1439,6 +1439,31 @@ static const struct panel_desc innolux_zj070na_01p = { }, }; +static const struct drm_display_mode jenson_1024x600jt60396_01_mode = { + .clock = 51200, + .hdisplay = 1024, + .hsync_start = 1024 + 0, + .hsync_end = 1024 + 0 + 320, + .htotal = 1024 + 0 + 320 + 0, + .vdisplay = 600, + .vsync_start = 600 + 0, + .vsync_end = 600 + 0 + 35, + .vtotal = 600 + 0 + 35 + 0, + .vrefresh = 60, + .flags = DRM_MODE_FLAG_NHSYNC | DRM_MODE_FLAG_NVSYNC, +}; + +static const struct panel_desc jenson_1024x600jt60396_01 = { + .modes = &jenson_1024x600jt60396_01_mode, + .num_modes = 1, + .bpc = 8, + .size = { + .width = 154, + .height = 85, + }, + .bus_format = MEDIA_BUS_FMT_RGB888_1X24, +}; + static const struct display_timing koe_tx31d200vm0baa_timing = { .pixelclock = { 39600000, 43200000, 48000000 }, .hactive = { 1280, 1280, 1280 }, @@ -2480,6 +2505,9 @@ static const struct of_device_id platform_of_match[] = { .compatible = "innolux,zj070na-01p", .data = &innolux_zj070na_01p, }, { + .compatible = "jenson,jt60396-01", + .data = &jenson_1024x600jt60396_01, + }, { .compatible = "koe,tx31d200vm0baa", .data = &koe_tx31d200vm0baa, }, {
View more

The build process ends correctly but the boot log shows the following errors

[11066.089809] [drm:drm_atomic_helper_wait_for_dependencies] *ERROR* [CRTC:32:crtc-0] flip_done timed out [11076.329852] [drm:drm_atomic_helper_wait_for_dependencies] *ERROR* [CONNECTOR:29:DPI-1] flip_done timed out [11086.569810] [drm:drm_atomic_helper_wait_for_dependencies] *ERROR* [PLANE:30:plane-0] flip_done timed out

 and the display screen doesn't show anything

Any suggestion?

Thanks

0 REPLIES 0