2020-07-09 1:18 AM
The program can not be uploaded under the dunfell distribution via CUBEIDE 1.3.1 to the target system. Using the thud distribution, target uploads works.
Are there any hidden upload scripts in the CUBEIDE - how to debug the debug upload?
Which yocto packages are necessary to cooperate with the CUBEIDE?
Solved! Go to Solution.
2020-07-17 7:32 AM
Hi,
The fix is now published.
https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v2.0.0
https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note_-_v2.0.0
some cipher methods have been disabled by the community for security reasons.
As a consequence some ssh requests from STM32CubeIDE may not be functional due to the dropbear package configuration.
In this case, you can either:
Best Regards,
Olivier
2020-07-09 1:22 AM
Hi @meiss.M
Just did some trials of loading M4 example code from CubeIDE1.3.1 with dunfell Starter Package and it works.
Could you share more precisely error you face ?
Thanks
Olivier
2020-07-09 1:37 AM
When looking in the /lib/firmware directory on the target, there is no uploaded elf file.
If I upload it by hand, load it into the co-processor, gdb seems to connect.
It is mainly because of the target upload.
On the thud distribution running on the target, the "Uploading to target process indication" flops up. This did not happen using my built using the dunfell distribution.
Is the CUBEIDE uploading via ssh scp?
Which yocto packages are necessary to cooperate with the CUBEIDE?
2020-07-09 1:54 AM
Hi @meiss.M
Yes in "production mode" CubeIDE upload elf via ssh connection.
Not change here between thud and dunfell.
Which connection did you set between Host and target ? Ethernet Over USB ? Point to point or LAN ? Behind swith or proxy ?
Any error message from CubeIDE when starting debug ?
>> On the thud distribution running on the target, the "Uploading to target process indication" flops up
This is confusing me. What do you mean ?
Olivier
2020-07-09 2:00 AM
Messages on the CubeIDE is:
I am using ethernet via a different network, DHCP.
However for the thud build, I am using the same ethernet setup and it worked.
No source available for "g_pfnVectors() at 0x0"
It seems there were no shell commands executed on the target.
2020-07-09 2:04 AM
Thanks @meiss.M
Could be interesting to get the OpenOCD console traces please
Olivier
2020-07-09 2:14 AM
>> On the thud distribution running on the target, the "Uploading to target process indication" flops up
This is confusing me. What do you mean ?
This is the process indicator when using the the thud build on the target.
On dunfell I do not get so far. - Same network configuration, CUBEIDE was not restarted after target upload failure on the dunfell built.
2020-07-09 2:28 AM
OPENOCD Trace on the dunfell build:
Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:54)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
cortex_a interrupt mask on
cortex_a interrupt mask on
cortex_a domain access control fixup on
cortex_a domain access control fixup on
none separate
adapter speed: 8000 kHz
adapter_nsrst_assert_width: 200
adapter_nsrst_delay: 200
none srst_pulls_trst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J36S26 (API v2) VID:PID 0483:3752
Info : using stlink api v2
Info : Target voltage: 3.246134
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : SRST line released
Info : stlink_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP157CACx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157CACx.cpu1: hardware has 6 breakpoints, 4 watchpoints
Error: Could not find MEM-AP to control the core
Info : Listening on port 3334 for gdb connections
Info : Listening on port 3333 for gdb connections
ap 0 selected, csw 0x10006000
Info : accepting 'gdb' connection on tcp/3333
Error: Target not examined yet
Info : New GDB Connection: 1, Target STM32MP157CACx.cpu2, state: unknown
undefined debug reason 7 - target needs reset
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Warn : target STM32MP157CACx.cpu2 is not halted (add breakpoint)
Error: can't add breakpoint: target running
Error: Target not examined yet
Error: Target not examined yet
ap 0 selected, csw 0x10006000
shutdown command invoked
Info : dropped 'gdb' connection
2020-07-09 2:36 AM
Should I build my yocto with the previous openocd from thud?
Do you think this is an option?
2020-07-09 3:06 AM
Hi @meiss.M
I understand you use a dunfell image built with Distribution package ?
Can you make a try with the delivered Starter Package ?
Are you under windows or Ubuntu ?
If Ubuntu can you please share content of /etc/udev/rules.d/49-stlinkv2-1.rules ?
Thx,
Olivier